<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: output pin state at power up in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/output-pin-state-at-power-up/m-p/129373#M1931</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi, irob:&lt;BR /&gt;&lt;BR /&gt;From the time reset asserts (or power is applied) until you write the DDR, the pins are inputs, and might float wherever they please.&lt;BR /&gt;&lt;BR /&gt;The only way that I know to make them behave during reset is to use either a pull-up or pull-down resistor. 10k is my favorite value, but it depends on what is being driven by the pin.&lt;BR /&gt;&lt;BR /&gt;My experience is that it is usually the not-yet-driven input that determines in which direction the net floats, due to leakage current.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Sep 2006 05:20:10 GMT</pubDate>
    <dc:creator>rocco</dc:creator>
    <dc:date>2006-09-07T05:20:10Z</dc:date>
    <item>
      <title>output pin state at power up</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/output-pin-state-at-power-up/m-p/129372#M1930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hey gang,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone know how to set the level of output pins during power up? For instance, I have a few outputs which crucially must remain low during power up until I set them as outputs, and start to use them.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If memory serves, back in the 68HC11 days one had to set the pins in question to the desired state &lt;/SPAN&gt;&lt;EM&gt;before&lt;/EM&gt;&lt;SPAN&gt; setting their direction registers.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've done this (setting pins low before their DDRs) and somewhat arbitrarily one of my outputs wants to float high while another floats low.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any ideas?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Sep 2006 03:42:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/output-pin-state-at-power-up/m-p/129372#M1930</guid>
      <dc:creator>irob</dc:creator>
      <dc:date>2006-09-07T03:42:20Z</dc:date>
    </item>
    <item>
      <title>Re: output pin state at power up</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/output-pin-state-at-power-up/m-p/129373#M1931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi, irob:&lt;BR /&gt;&lt;BR /&gt;From the time reset asserts (or power is applied) until you write the DDR, the pins are inputs, and might float wherever they please.&lt;BR /&gt;&lt;BR /&gt;The only way that I know to make them behave during reset is to use either a pull-up or pull-down resistor. 10k is my favorite value, but it depends on what is being driven by the pin.&lt;BR /&gt;&lt;BR /&gt;My experience is that it is usually the not-yet-driven input that determines in which direction the net floats, due to leakage current.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Sep 2006 05:20:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/output-pin-state-at-power-up/m-p/129373#M1931</guid>
      <dc:creator>rocco</dc:creator>
      <dc:date>2006-09-07T05:20:10Z</dc:date>
    </item>
  </channel>
</rss>