<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: problem i execting the  stop3 using RTC in MC9S08SH8 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/problem-i-execting-the-stop3-using-RTC-in-MC9S08SH8/m-p/220656#M19178</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Disclaimer: &amp;nbsp;I'm an amateur at best.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In your ISR, you have:&lt;/P&gt;&lt;P&gt;RTCSC_RTIF = 1;&lt;/P&gt;&lt;P&gt;RTCSC_RTIE = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Both of these are wrong I believe. &amp;nbsp;Instead you should use simply:&lt;/P&gt;&lt;P&gt;RTCSC_RTIACK=1; &amp;nbsp; //Clears the RTIF bit and clears the interrupt request&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(You do not need the second line at all, unless you want to actually turn off the RTI altogether (ie. trigger no further interrupts). &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In your code somewhere (not in the ISR) you have to have&amp;nbsp;&lt;/P&gt;&lt;P&gt;RTCSC_RTIE = 1; &amp;nbsp;//Enable the RTI to begin with&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps, not sure if I'm missing something here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Sep 2010 20:21:00 GMT</pubDate>
    <dc:creator>PatrickW</dc:creator>
    <dc:date>2010-09-09T20:21:00Z</dc:date>
    <item>
      <title>problem i execting the  stop3 using RTC in MC9S08SH8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/problem-i-execting-the-stop3-using-RTC-in-MC9S08SH8/m-p/220655#M19177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi...&lt;/P&gt;&lt;P&gt;i'm using RTC for waking the stop-3 mode. and i'm using MC9S08SH8 8-bit microcontroller in my application.&lt;/P&gt;&lt;P&gt;and the initialisations are:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;#define &amp;nbsp; x &amp;nbsp; 0x01&lt;/P&gt;&lt;P&gt;#define&amp;nbsp;&amp;nbsp; y&amp;nbsp;&amp;nbsp; 0xFE&lt;/P&gt;&lt;P&gt;main()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; for( ; ; )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RTCSC = 0x1F;&amp;nbsp; //1sec&amp;nbsp; 1khz clock source is enabled.with RTIE enabled&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if( Z &amp;amp; x)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //refer above for x&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Z = Z&amp;nbsp; &amp;amp; y;&amp;nbsp;&amp;nbsp;&amp;nbsp; //refer above for y&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _Stop;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __RESET_WATCHDOG(); /* feeds the dog */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;void interrupt VectorNumber_Vtpm1ovf timerPWM(void)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt; //timer interrpt for 0.1sec&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TPM1SC_TOF=0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTAD_PTAD2 = ~ PTAD_PTAD2; //for checking purpose&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Z = 0x01;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;void interrupt VectorNumber_Vrtc&amp;nbsp; realtimeinterrupt(void)&lt;/STRONG&gt;&lt;BR /&gt;{ &amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RTCSC_RTIF = 1; //for clearing RTIF flag.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RTCSC_RTIE = 0;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the above case, RTC not waking properly, and the two ISR's are not working exactly. so, please ttell me where the problem is occuring.i.e, when the stop instruction in the for loop is seen, it enter into stop and after one sec, RTC interrupt comes, because i uased 1KHz clock source. and the RTC interrupt flag clear , and after that bus_clock everything has to work normally but &lt;STRONG&gt;it is not going to timer PWM ISR immediately&lt;/STRONG&gt; it is taking large time to go to timer interrupt. so, im thinking some wrong i'm making in the initialisation.&lt;/P&gt;&lt;P&gt;In case of enabling the RTC , initialisation is sufficient or anything has to be done. and 1KHz source can be used for RTC to wake from STOP-3 mode. and please provide the solution for the above problem as early as possible.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Sep 2010 02:01:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/problem-i-execting-the-stop3-using-RTC-in-MC9S08SH8/m-p/220655#M19177</guid>
      <dc:creator>ellendula</dc:creator>
      <dc:date>2010-09-05T02:01:53Z</dc:date>
    </item>
    <item>
      <title>Re: problem i execting the  stop3 using RTC in MC9S08SH8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/problem-i-execting-the-stop3-using-RTC-in-MC9S08SH8/m-p/220656#M19178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Disclaimer: &amp;nbsp;I'm an amateur at best.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In your ISR, you have:&lt;/P&gt;&lt;P&gt;RTCSC_RTIF = 1;&lt;/P&gt;&lt;P&gt;RTCSC_RTIE = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Both of these are wrong I believe. &amp;nbsp;Instead you should use simply:&lt;/P&gt;&lt;P&gt;RTCSC_RTIACK=1; &amp;nbsp; //Clears the RTIF bit and clears the interrupt request&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(You do not need the second line at all, unless you want to actually turn off the RTI altogether (ie. trigger no further interrupts). &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In your code somewhere (not in the ISR) you have to have&amp;nbsp;&lt;/P&gt;&lt;P&gt;RTCSC_RTIE = 1; &amp;nbsp;//Enable the RTI to begin with&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps, not sure if I'm missing something here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Sep 2010 20:21:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/problem-i-execting-the-stop3-using-RTC-in-MC9S08SH8/m-p/220656#M19178</guid>
      <dc:creator>PatrickW</dc:creator>
      <dc:date>2010-09-09T20:21:00Z</dc:date>
    </item>
    <item>
      <title>Re: problem i execting the  stop3 using RTC in MC9S08SH8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/problem-i-execting-the-stop3-using-RTC-in-MC9S08SH8/m-p/220657#M19179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Patrick,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;While other S08 devices have an RTIACK bit to acknowledge and clear the RTIF flag, this one does not.&lt;/P&gt;&lt;P&gt;Writing a 1 to RTIF is the correct method for clearing the RTIF flag here.&lt;/P&gt;&lt;P&gt;RTFM!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Sep 2010 04:46:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/problem-i-execting-the-stop3-using-RTC-in-MC9S08SH8/m-p/220657#M19179</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2010-09-10T04:46:27Z</dc:date>
    </item>
    <item>
      <title>Re: problem i execting the  stop3 using RTC in MC9S08SH8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/problem-i-execting-the-stop3-using-RTC-in-MC9S08SH8/m-p/220658#M19180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ah, see this is why I included disclaimers at the top and bottom divulging my non-professionalism!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;OP: &amp;nbsp;Sorry if that caused you additional confusion. &amp;nbsp;I only hazarded my attempt at assistance because nobody had responded to your question for awhile... this will teach me to leave advice-giving to the experts!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Sep 2010 16:27:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/problem-i-execting-the-stop3-using-RTC-in-MC9S08SH8/m-p/220658#M19180</guid>
      <dc:creator>PatrickW</dc:creator>
      <dc:date>2010-09-10T16:27:28Z</dc:date>
    </item>
  </channel>
</rss>