<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: How to exit Stop2 QE64?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-exit-Stop2-QE64/m-p/219770#M19136</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;IRQ pin can be used to wake-up MCU from Stop3, the signal could be active low or active high desided how you config the IRQEDG.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But when IRQ pin&amp;nbsp;is used to wake-up MCU from Stop2, the signal should be active_low only.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Oct 2009 14:12:49 GMT</pubDate>
    <dc:creator>vircom</dc:creator>
    <dc:date>2009-10-09T14:12:49Z</dc:date>
    <item>
      <title>How to exit Stop2 QE64?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-exit-Stop2-QE64/m-p/219769#M19135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can I exit STOP2 mode by going HIGH on the IRQ pin (If I have configured the IRQEDG = 1) IRQ is rising edge/high-level sensitive.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The manual on p.43 says&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;3.6.1.3 Exit from Stop2&lt;BR /&gt;Exit from stop2 is performed by &lt;STRONG&gt;asserting the wake-up&lt;/STRONG&gt; &lt;STRONG&gt;pin&lt;/STRONG&gt; (PTA5/IRQ/TCLK/RESET) on the MCU.&lt;BR /&gt;&lt;STRONG&gt;NOTE&lt;/STRONG&gt;&lt;BR /&gt;PTA5/IRQ/TPM1CLK/RESET functions as an &lt;STRONG&gt;active-low wakeup input&lt;/STRONG&gt;&lt;BR /&gt;when the MCU is in stop2. The pullup on this pin is not automatically&lt;BR /&gt;enabled in stop2. To enable the internal pullup, set the PTAPE5 bit in the&lt;BR /&gt;port A pull enable register (PTAPE).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;p.47 says&amp;nbsp; "&lt;STRONG&gt;Assert zero&lt;/STRONG&gt; on PTA5/IRQ/TPM1CLK/RESET" to Transition from STOP2 to RUN&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then p.93 says&lt;/P&gt;&lt;P&gt;5.5.2.1 Pin Configuration Options&lt;BR /&gt;...As an IRQ input, the user can choose the polarity of edges or levels detected...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and p.98 even has a register for the Edge Select IRQEDG&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Really misleading.&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Oct 2009 22:20:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-exit-Stop2-QE64/m-p/219769#M19135</guid>
      <dc:creator>Andrey</dc:creator>
      <dc:date>2009-10-07T22:20:46Z</dc:date>
    </item>
    <item>
      <title>Re: How to exit Stop2 QE64?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-exit-Stop2-QE64/m-p/219770#M19136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;IRQ pin can be used to wake-up MCU from Stop3, the signal could be active low or active high desided how you config the IRQEDG.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But when IRQ pin&amp;nbsp;is used to wake-up MCU from Stop2, the signal should be active_low only.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Oct 2009 14:12:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-exit-Stop2-QE64/m-p/219770#M19136</guid>
      <dc:creator>vircom</dc:creator>
      <dc:date>2009-10-09T14:12:49Z</dc:date>
    </item>
  </channel>
</rss>