<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollersのトピックprogramming adapter (PAS08W1628T28E) setup</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/programming-adapter-PAS08W1628T28E-setup/m-p/219643#M19127</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a PAS08W1628T28E programming adapter, this adapter is connected to a&lt;BR /&gt;P&amp;amp;E cyclone pro through MON08 interface. Also, the P&amp;amp;E cyclone pro is connected&lt;BR /&gt;to a PC USB port. The MCU is MC908QC8 (28 pin TSSOP). I have connected jumpers&lt;BR /&gt;from J3 to J6 on the programming adapter board (PAS08W1628T28) by one to one&lt;BR /&gt;connection (J3-1 to J6-1, J3-2 to J6-2,…….. J3-16 to J6-16). When I run&lt;BR /&gt;Codewarrior 6.2, it shows a message “Could not measure target baudrate”. P&amp;amp;E&lt;BR /&gt;Connection Manager window shows “Connection Status Summary YNNNN”. Have I&lt;BR /&gt;missed other jumper connections? what I have done wrong? P&amp;amp;E cyclone pro is&lt;BR /&gt;working correctly when it connects to a 908Q programming adapter (Slicon&lt;BR /&gt;Engines).&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;/P&gt;&lt;P&gt;aurora&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Aug 2010 19:26:19 GMT</pubDate>
    <dc:creator>aurora</dc:creator>
    <dc:date>2010-08-25T19:26:19Z</dc:date>
    <item>
      <title>programming adapter (PAS08W1628T28E) setup</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/programming-adapter-PAS08W1628T28E-setup/m-p/219643#M19127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a PAS08W1628T28E programming adapter, this adapter is connected to a&lt;BR /&gt;P&amp;amp;E cyclone pro through MON08 interface. Also, the P&amp;amp;E cyclone pro is connected&lt;BR /&gt;to a PC USB port. The MCU is MC908QC8 (28 pin TSSOP). I have connected jumpers&lt;BR /&gt;from J3 to J6 on the programming adapter board (PAS08W1628T28) by one to one&lt;BR /&gt;connection (J3-1 to J6-1, J3-2 to J6-2,…….. J3-16 to J6-16). When I run&lt;BR /&gt;Codewarrior 6.2, it shows a message “Could not measure target baudrate”. P&amp;amp;E&lt;BR /&gt;Connection Manager window shows “Connection Status Summary YNNNN”. Have I&lt;BR /&gt;missed other jumper connections? what I have done wrong? P&amp;amp;E cyclone pro is&lt;BR /&gt;working correctly when it connects to a 908Q programming adapter (Slicon&lt;BR /&gt;Engines).&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;/P&gt;&lt;P&gt;aurora&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Aug 2010 19:26:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/programming-adapter-PAS08W1628T28E-setup/m-p/219643#M19127</guid>
      <dc:creator>aurora</dc:creator>
      <dc:date>2010-08-25T19:26:19Z</dc:date>
    </item>
    <item>
      <title>Re: programming adapter (PAS08W1628T28E) setup</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/programming-adapter-PAS08W1628T28E-setup/m-p/219644#M19128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem has resolved.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Aurora&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Aug 2010 23:28:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/programming-adapter-PAS08W1628T28E-setup/m-p/219644#M19128</guid>
      <dc:creator>aurora</dc:creator>
      <dc:date>2010-08-25T23:28:17Z</dc:date>
    </item>
  </channel>
</rss>