<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PART NO . MC908AB32CFUE   (need help) in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PART-NO-MC908AB32CFUE-need-help/m-p/219045#M19070</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A few S08 devices are stil available in DIP packages, mainly for lower pin count packages.&amp;nbsp; The closest to your needs would probably be the S08GT60 or S08GT32, which is available in a 42-pin shrink DIP package.&amp;nbsp; However, this device does not contain EEPROM, and&amp;nbsp;is limited to&amp;nbsp;four TPM channels.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Other S08 devices are available in SOIC packages, up to a maximum of 28 pins.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Aug 2010 23:05:11 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2010-08-19T23:05:11Z</dc:date>
    <item>
      <title>PART NO . MC908AB32CFUE   (need help)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PART-NO-MC908AB32CFUE-need-help/m-p/219043#M19068</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;partno.MC908AB32CFUE&amp;nbsp; available in QFP package&amp;nbsp; ..&lt;/P&gt;&lt;P&gt;can any one tell me that there are any DIP or SOIC package available of same MCU .&lt;/P&gt;&lt;P&gt;the development work on QFP package is difficult plz suggest me.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Aug 2010 13:47:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PART-NO-MC908AB32CFUE-need-help/m-p/219043#M19068</guid>
      <dc:creator>wasimakram</dc:creator>
      <dc:date>2010-08-19T13:47:33Z</dc:date>
    </item>
    <item>
      <title>Re: PART NO . MC908AB32CFUE   (need help)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PART-NO-MC908AB32CFUE-need-help/m-p/219044#M19069</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the manual, the chip only comes in LQFP 64. Unfortunately that's how all MCUs look today, the DIP days are over.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A sidenote: if you are developing a brand new product, you shouldn't use an old 68HC08. The S08 is a newer, better MCU and code compatible with 68HC08.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Aug 2010 15:18:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PART-NO-MC908AB32CFUE-need-help/m-p/219044#M19069</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2010-08-19T15:18:36Z</dc:date>
    </item>
    <item>
      <title>Re: PART NO . MC908AB32CFUE   (need help)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PART-NO-MC908AB32CFUE-need-help/m-p/219045#M19070</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A few S08 devices are stil available in DIP packages, mainly for lower pin count packages.&amp;nbsp; The closest to your needs would probably be the S08GT60 or S08GT32, which is available in a 42-pin shrink DIP package.&amp;nbsp; However, this device does not contain EEPROM, and&amp;nbsp;is limited to&amp;nbsp;four TPM channels.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Other S08 devices are available in SOIC packages, up to a maximum of 28 pins.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Aug 2010 23:05:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PART-NO-MC908AB32CFUE-need-help/m-p/219045#M19070</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-08-19T23:05:11Z</dc:date>
    </item>
    <item>
      <title>Re: PART NO . MC908AB32CFUE   (need help)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PART-NO-MC908AB32CFUE-need-help/m-p/219046#M19071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;However if you wanna be attached to that PN, you could use an adapter.&lt;/P&gt;&lt;P&gt;These anything-to-100mils pinhead adapters (one for each side of the package) are still in use for prototypes.&lt;/P&gt;&lt;P&gt;If you check JM60 Flexis demo board, you'll get the picture.&lt;/P&gt;&lt;P&gt;You can find these cheap&amp;amp;durty adapters in ebay.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope it helps,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Celso&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Aug 2010 23:15:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PART-NO-MC908AB32CFUE-need-help/m-p/219046#M19071</guid>
      <dc:creator>celsoken</dc:creator>
      <dc:date>2010-08-19T23:15:02Z</dc:date>
    </item>
    <item>
      <title>Re: PART NO . MC908AB32CFUE   (need help)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PART-NO-MC908AB32CFUE-need-help/m-p/219047#M19072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello&lt;/P&gt;&lt;P&gt;thanx 4 suggetion&lt;/P&gt;&lt;P&gt;but our bond with MC908AB332&lt;/P&gt;&lt;P&gt;SO,conclusion is this ,i have to work on QFP package and there are no any DIP or SOIC package?&lt;/P&gt;&lt;P&gt;and if i am right? then the debugger for this part is MON-08 MULTILINK with USB-16 PIN (FEMALE) OUT&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Aug 2010 13:50:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PART-NO-MC908AB32CFUE-need-help/m-p/219047#M19072</guid>
      <dc:creator>wasimakram</dc:creator>
      <dc:date>2010-08-20T13:50:37Z</dc:date>
    </item>
    <item>
      <title>Re: PART NO . MC908AB32CFUE   (need help)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PART-NO-MC908AB32CFUE-need-help/m-p/219048#M19073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, that's it! MON08 is the tool you need.&lt;/P&gt;&lt;P&gt;Good luck,&lt;/P&gt;&lt;P&gt;Celso&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Aug 2010 18:51:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PART-NO-MC908AB32CFUE-need-help/m-p/219048#M19073</guid>
      <dc:creator>celsoken</dc:creator>
      <dc:date>2010-08-20T18:51:01Z</dc:date>
    </item>
    <item>
      <title>Re: PART NO . MC908AB32CFUE   (need help)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/PART-NO-MC908AB32CFUE-need-help/m-p/219049#M19074</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks all&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Aug 2010 14:05:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/PART-NO-MC908AB32CFUE-need-help/m-p/219049#M19074</guid>
      <dc:creator>wasimakram</dc:creator>
      <dc:date>2010-08-21T14:05:28Z</dc:date>
    </item>
  </channel>
</rss>