<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックTPM2CLK Input Not Getting Pulled Up (AC32)</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM2CLK-Input-Not-Getting-Pulled-Up-AC32/m-p/218781#M19056</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using an 'AC32 part and want to use an external clock source for TPM2.&amp;nbsp; I have an open collector driver currently driving that port pin (PTD4/TPM2CLK/AD1P12) and it is pulled up internally.&amp;nbsp; When used just as an input port with the internal pull-up enabled, it works fine (i.e. the pullup works).&amp;nbsp; When used as an external clock input, the pull-up does not seem to be there.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The manual states, "When any pin associated with the timer is configured as a timer input, a passive pullup can be enabled."&amp;nbsp; That sounds like my pull-up should work.&amp;nbsp; My internal pull-up is still enabled, but it does not pull the pin high when configured as TPM2CLK.&amp;nbsp; Any clues?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Lou&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Sep 2009 04:22:38 GMT</pubDate>
    <dc:creator>Luigi</dc:creator>
    <dc:date>2009-09-30T04:22:38Z</dc:date>
    <item>
      <title>TPM2CLK Input Not Getting Pulled Up (AC32)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM2CLK-Input-Not-Getting-Pulled-Up-AC32/m-p/218781#M19056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using an 'AC32 part and want to use an external clock source for TPM2.&amp;nbsp; I have an open collector driver currently driving that port pin (PTD4/TPM2CLK/AD1P12) and it is pulled up internally.&amp;nbsp; When used just as an input port with the internal pull-up enabled, it works fine (i.e. the pullup works).&amp;nbsp; When used as an external clock input, the pull-up does not seem to be there.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The manual states, "When any pin associated with the timer is configured as a timer input, a passive pullup can be enabled."&amp;nbsp; That sounds like my pull-up should work.&amp;nbsp; My internal pull-up is still enabled, but it does not pull the pin high when configured as TPM2CLK.&amp;nbsp; Any clues?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Lou&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Sep 2009 04:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM2CLK-Input-Not-Getting-Pulled-Up-AC32/m-p/218781#M19056</guid>
      <dc:creator>Luigi</dc:creator>
      <dc:date>2009-09-30T04:22:38Z</dc:date>
    </item>
    <item>
      <title>Re: TPM2CLK Input Not Getting Pulled Up (AC32)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM2CLK-Input-Not-Getting-Pulled-Up-AC32/m-p/218782#M19057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm pretty sure the manual is referring to the timer channels (for input compare) and not the external timer clock input. If that is a direct quote from a manual then i would agree that the phrase is misleading.&lt;/P&gt;&lt;P&gt;The current ACxx manual appears to be a little bit clearer in this description.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;JD&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Oct 2009 13:40:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM2CLK-Input-Not-Getting-Pulled-Up-AC32/m-p/218782#M19057</guid>
      <dc:creator>ThaManJD</dc:creator>
      <dc:date>2009-10-06T13:40:46Z</dc:date>
    </item>
    <item>
      <title>Re: TPM2CLK Input Not Getting Pulled Up (AC32)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM2CLK-Input-Not-Getting-Pulled-Up-AC32/m-p/218783#M19058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I finally got the answer from my Freescale rep who contacted the factory.&amp;nbsp; It is as you say.&amp;nbsp; The timer "inputs" as they say that still have pull-ups enabled are only those used when doing capture.&amp;nbsp; The documentation is VERY misleading and should be changed.&amp;nbsp; Thanks for the reply.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Oct 2009 19:46:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM2CLK-Input-Not-Getting-Pulled-Up-AC32/m-p/218783#M19058</guid>
      <dc:creator>Luigi</dc:creator>
      <dc:date>2009-10-08T19:46:51Z</dc:date>
    </item>
    <item>
      <title>Re: TPM2CLK Input Not Getting Pulled Up (AC32)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM2CLK-Input-Not-Getting-Pulled-Up-AC32/m-p/218784#M19059</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the exact name of the Freescale document you were using that was not clear on the subject? I am trying to report this problem so that it can be fixed and prevent this from happening in the future.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Oct 2009 20:39:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM2CLK-Input-Not-Getting-Pulled-Up-AC32/m-p/218784#M19059</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2009-10-09T20:39:02Z</dc:date>
    </item>
    <item>
      <title>Re: TPM2CLK Input Not Getting Pulled Up (AC32)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM2CLK-Input-Not-Getting-Pulled-Up-AC32/m-p/218785#M19060</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry for the delay in getting back to you.&amp;nbsp; On both the front and back of the document it says, "MC9S08AW60, Rev 2 12/2006".&amp;nbsp; Thanks for reporting it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Lou&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Oct 2009 02:35:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM2CLK-Input-Not-Getting-Pulled-Up-AC32/m-p/218785#M19060</guid>
      <dc:creator>Luigi</dc:creator>
      <dc:date>2009-10-22T02:35:39Z</dc:date>
    </item>
  </channel>
</rss>