<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: L1119 Error</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Error/m-p/218298#M19001</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got you. Thanks Mac&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Jul 2011 21:59:54 GMT</pubDate>
    <dc:creator>Idontunderstand</dc:creator>
    <dc:date>2011-07-01T21:59:54Z</dc:date>
    <item>
      <title>L1119 Error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Error/m-p/218293#M18996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi;&lt;/P&gt;&lt;P&gt;I wrote a code for MC9S12C128 micro-controller two years ago, now I need those code again and tried to run it, it gave me strange error. By googleing it I couldn't solve it.&lt;/P&gt;&lt;P&gt;Why I have this error, since this code worked fine before?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The error is:&lt;/P&gt;&lt;P&gt;Link Error: L119: Vector allocated at absolute address 0xFFFE overlaps with sections placed in segment. absSeg221&lt;/P&gt;&lt;P&gt;Link Error: Link failed&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;please help me how can i fix it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks;&lt;/P&gt;&lt;P&gt;Sb&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jun 2011 00:51:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Error/m-p/218293#M18996</guid>
      <dc:creator>Idontunderstand</dc:creator>
      <dc:date>2011-06-30T00:51:01Z</dc:date>
    </item>
    <item>
      <title>Re: L1119 Error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Error/m-p/218294#M18997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sb,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I suspect that your reset vector is specified in two places, in a vector table within your code, and also within the PRM file.&amp;nbsp; If this is the case, comment out the entry in the PRM file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jun 2011 08:02:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Error/m-p/218294#M18997</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-06-30T08:02:07Z</dc:date>
    </item>
    <item>
      <title>Re: L1119 Error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Error/m-p/218295#M18998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for response.&lt;/P&gt;&lt;P&gt;where is &amp;nbsp;PRM file﻿? could you tell me more specific?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jul 2011 01:39:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Error/m-p/218295#M18998</guid>
      <dc:creator>Idontunderstand</dc:creator>
      <dc:date>2011-07-01T01:39:08Z</dc:date>
    </item>
    <item>
      <title>Re: L1119 Error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Error/m-p/218296#M18999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found PRM folder,there are two files with prm extension. did you talk about these files? then what do u mean by comment it?&lt;/P&gt;&lt;P&gt;There is only one reset vector defined...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jul 2011 02:01:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Error/m-p/218296#M18999</guid>
      <dc:creator>Idontunderstand</dc:creator>
      <dc:date>2011-07-01T02:01:19Z</dc:date>
    </item>
    <item>
      <title>Re: L1119 Error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Error/m-p/218297#M19000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The file &lt;STRONG&gt;project.prm&lt;/STRONG&gt; is the one of interest.&amp;nbsp; At the end of the file, there should be a line containing something like the following entry:&lt;/P&gt;&lt;P&gt;&lt;FONT color="#ff0000" face="courier new,courier"&gt;VECTOR 0 _Startup /* Reset vector: this is the default entry point for an application. */&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Modify this as follows, so that the line is treated as a comment only.&lt;/P&gt;&lt;P&gt;&lt;FONT color="#ff0000" face="courier new,courier"&gt;//VECTOR 0 _Startup /* Reset vector: this is the default entry point for an application. */&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;This is often preferred to removing the line altogether, so that it remains apparent where the standard file has been edited.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jul 2011 14:41:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Error/m-p/218297#M19000</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-07-01T14:41:06Z</dc:date>
    </item>
    <item>
      <title>Re: L1119 Error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Error/m-p/218298#M19001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got you. Thanks Mac&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jul 2011 21:59:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Error/m-p/218298#M19001</guid>
      <dc:creator>Idontunderstand</dc:creator>
      <dc:date>2011-07-01T21:59:54Z</dc:date>
    </item>
  </channel>
</rss>