<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 How to create a project including two targets in CodeWarrior</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-create-a-project-including-two-targets-in-CodeWarrior/m-p/123828#M19</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Dear everybody,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to creat a project including two targets in Metrowerk's CodeWarrior. How to do that? How to associate the code corresponding with each target ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Jul 2006 14:51:55 GMT</pubDate>
    <dc:creator>baonguyen</dc:creator>
    <dc:date>2006-07-12T14:51:55Z</dc:date>
    <item>
      <title>How to create a project including two targets in CodeWarrior</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-create-a-project-including-two-targets-in-CodeWarrior/m-p/123828#M19</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Dear everybody,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to creat a project including two targets in Metrowerk's CodeWarrior. How to do that? How to associate the code corresponding with each target ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jul 2006 14:51:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-create-a-project-including-two-targets-in-CodeWarrior/m-p/123828#M19</guid>
      <dc:creator>baonguyen</dc:creator>
      <dc:date>2006-07-12T14:51:55Z</dc:date>
    </item>
    <item>
      <title>Re: How to create a project including two targets in CodeWarrior</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-create-a-project-including-two-targets-in-CodeWarrior/m-p/123829#M20</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;it's simple.&lt;/P&gt;&lt;P&gt;Click on &lt;FONT color="#ff0000"&gt;target menu&lt;/FONT&gt;.&lt;/P&gt;&lt;P&gt;Choose one target.&lt;/P&gt;&lt;P&gt;go to &lt;FONT color="#ff0000"&gt;project--&amp;gt;Create target.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;here you can &lt;FONT color="#ff0000"&gt;clone the target&lt;/FONT&gt; or create a &lt;FONT color="#ff0000"&gt;new target&lt;/FONT&gt;.&lt;/P&gt;&lt;P&gt;if you are cloning you have to change the name &lt;FONT color="#ff0000"&gt;twice in target settings&lt;/FONT&gt;.&lt;/P&gt;&lt;P&gt;then add the files required for the target.&lt;/P&gt;&lt;P&gt;you can remove the files from any target using &lt;FONT color="#ff0000"&gt;project inspector.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Fire&lt;/P&gt;&lt;P&gt;&lt;FONT color="#ff0000"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#ff0000"&gt;&lt;/FONT&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jul 2006 10:26:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/How-to-create-a-project-including-two-targets-in-CodeWarrior/m-p/123829#M20</guid>
      <dc:creator>fire</dc:creator>
      <dc:date>2006-07-14T10:26:32Z</dc:date>
    </item>
  </channel>
</rss>