<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: link  error :1102 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/link-error-1102/m-p/218114#M18980</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unless you have been messing around in the .PRM file, it would seem that the RAM is full. Check the map file for details of how much memory everything things take up and where they are allocated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This can only be solved by using fewer global/static variables. Or alternatively upgrade to a device with bigger RAM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Aug 2010 16:29:00 GMT</pubDate>
    <dc:creator>Lundin</dc:creator>
    <dc:date>2010-08-13T16:29:00Z</dc:date>
    <item>
      <title>link  error :1102</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/link-error-1102/m-p/218113#M18979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;I&amp;nbsp; am using code warrier v6.3, and runnig&amp;nbsp; motor controller code (DMR115 ),&lt;/P&gt;&lt;P&gt;&amp;nbsp;when&amp;nbsp;&amp;nbsp;&amp;nbsp; coplile then it shws error&amp;nbsp; like&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Link Error: L1102 : out of allocation space in segment&amp;nbsp; RAM at adress : 0x425,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;please tell hoew to overcome&amp;nbsp; to this error&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Aug 2010 15:07:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/link-error-1102/m-p/218113#M18979</guid>
      <dc:creator>Arhan</dc:creator>
      <dc:date>2010-08-13T15:07:39Z</dc:date>
    </item>
    <item>
      <title>Re: link  error :1102</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/link-error-1102/m-p/218114#M18980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unless you have been messing around in the .PRM file, it would seem that the RAM is full. Check the map file for details of how much memory everything things take up and where they are allocated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This can only be solved by using fewer global/static variables. Or alternatively upgrade to a device with bigger RAM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Aug 2010 16:29:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/link-error-1102/m-p/218114#M18980</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2010-08-13T16:29:00Z</dc:date>
    </item>
    <item>
      <title>Re: link  error :1102</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/link-error-1102/m-p/218115#M18981</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Further to Lundin's comment,&amp;nbsp;if your program uses the default allocation for placement of global and static variables, it is&amp;nbsp;possible that zero page RAM will not be utilized.&amp;nbsp; If this is the case, you can gain some additional RAM space by allocating some ot the variables wthin zero page.&amp;nbsp; You will need to use the appropriate pragmas to achieve this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The memory available for global and static variables will also be balanced against the stack size.&amp;nbsp; If the stack size allowed is over-generous, you might consider its reduction.&amp;nbsp; But you will need to experimentally determine the actual&amp;nbsp;stack requirements of the program for a worst case situation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are you using the MCU type&amp;nbsp;that DMR115 was intended to operate with, or a smaller device?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Aug 2010 23:02:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/link-error-1102/m-p/218115#M18981</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-08-13T23:02:24Z</dc:date>
    </item>
  </channel>
</rss>