<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: Unused IRQ Pin Termination</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unused-IRQ-Pin-Termination-MC9S08AW32/m-p/217624#M18949</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;If you want to use the IRQ pin, as an IRQ, set the IRQPE bit om the&amp;nbsp;IRQSC register to 1.&lt;/DIV&gt;&lt;DIV&gt;If you have set the IRQPE pin, you can select if you want to have falling or rising edge triggering the IRQ interrupt, by clearing setting IRQEDG bit.&lt;/DIV&gt;&lt;DIV&gt;The IRQPE is cleared as default, so initially the IRQ interrupt is disabled.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If you don't want to use the IRQ pin at all, I would connect a 10 kOhm pullup resistor and a 0.1 uF capacitor to the IRQ pin, and not write anything to the IRQSC register.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Did that answer your question?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Ake&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Jan 2009 16:43:58 GMT</pubDate>
    <dc:creator>Ake</dc:creator>
    <dc:date>2009-01-21T16:43:58Z</dc:date>
    <item>
      <title>Unused IRQ Pin Termination - MC9S08AW32</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unused-IRQ-Pin-Termination-MC9S08AW32/m-p/217623#M18948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-size: 2;"&gt;I am using an MC9S08AW32 processor and I will not be using the IRQ function.&amp;nbsp; I need to know how to terminate the unused pin.&amp;nbsp; The literature is a bit confusing in that it describes that an "optional" internal pull-up or pull-down resistor can be used.&amp;nbsp; It says, "&lt;SPAN style=": ; font-family: Helvetica;"&gt;&lt;EM&gt;&lt;SPAN style="font-family: Arial;"&gt;when this [IRQPE] bit is set&lt;/SPAN&gt;, either an internal pull-up or an internal pull-down resistor is enabled depending on the state of the IRQEDG bit&lt;/EM&gt;."&amp;nbsp; Does that mean when IRQPE = 0 there is no internal resistor selected?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Helvetica; font-size: 2;"&gt;I just need to know whether to pull the pin low externally or not.&amp;nbsp; I guess I could just do that, but I was not sure if an internal resistor was also active.&amp;nbsp; Suggestions?&amp;nbsp; Thanks.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Helvetica; font-size: 2;"&gt;Lou&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="font-family: Helvetica; font-size: 2;"&gt;Added p/n to subject.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by NLFSJ on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2009-01-26&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;07:56 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2009 23:01:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Unused-IRQ-Pin-Termination-MC9S08AW32/m-p/217623#M18948</guid>
      <dc:creator>Luigi</dc:creator>
      <dc:date>2009-01-20T23:01:20Z</dc:date>
    </item>
    <item>
      <title>Re: Unused IRQ Pin Termination</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unused-IRQ-Pin-Termination-MC9S08AW32/m-p/217624#M18949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;If you want to use the IRQ pin, as an IRQ, set the IRQPE bit om the&amp;nbsp;IRQSC register to 1.&lt;/DIV&gt;&lt;DIV&gt;If you have set the IRQPE pin, you can select if you want to have falling or rising edge triggering the IRQ interrupt, by clearing setting IRQEDG bit.&lt;/DIV&gt;&lt;DIV&gt;The IRQPE is cleared as default, so initially the IRQ interrupt is disabled.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If you don't want to use the IRQ pin at all, I would connect a 10 kOhm pullup resistor and a 0.1 uF capacitor to the IRQ pin, and not write anything to the IRQSC register.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Did that answer your question?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Ake&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jan 2009 16:43:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Unused-IRQ-Pin-Termination-MC9S08AW32/m-p/217624#M18949</guid>
      <dc:creator>Ake</dc:creator>
      <dc:date>2009-01-21T16:43:58Z</dc:date>
    </item>
    <item>
      <title>Re: Unused IRQ Pin Termination</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unused-IRQ-Pin-Termination-MC9S08AW32/m-p/217625#M18950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;The second half of what you wrote did.&amp;nbsp; Is your answer based on what Freescale has said about the pin, or your own best guess?&amp;nbsp; I am just curious if anyone knows for sure if this pin truly floats if it is not used.&amp;nbsp; I will default to pulling it high unless I hear otherwise, but I wondered if anyone else had investigated this.&amp;nbsp; Thanks.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Lou&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2009 01:29:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Unused-IRQ-Pin-Termination-MC9S08AW32/m-p/217625#M18950</guid>
      <dc:creator>Luigi</dc:creator>
      <dc:date>2009-01-23T01:29:47Z</dc:date>
    </item>
  </channel>
</rss>