<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Problems with jb16.</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-jb16/m-p/217265#M18927</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks, for your help. I proved all that you tell me but I am not sure about the&lt;BR /&gt;conection D+ and D-. bye&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by nic on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-09-21&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;05:15 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Sep 2009 23:11:49 GMT</pubDate>
    <dc:creator>nic</dc:creator>
    <dc:date>2009-09-21T23:11:49Z</dc:date>
    <item>
      <title>Problems with jb16.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-jb16/m-p/217263#M18925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need help, I can't install the drivers por icp programming. I use Windows xp sp2, is this a problem?.&lt;/P&gt;&lt;P&gt;My hardware is ok, Pta0 = 0v, two resistors (470K) pulldown on D+ and D-. If someone can help, thanks.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Sep 2009 01:59:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-jb16/m-p/217263#M18925</guid>
      <dc:creator>nic</dc:creator>
      <dc:date>2009-09-21T01:59:40Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with jb16.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-jb16/m-p/217264#M18926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Nic,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Your description is a bit vague!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Do you mean&lt;/P&gt;&lt;P&gt;1) that the device is not starting in ICP&lt;/P&gt;&lt;P&gt;&amp;nbsp; or&lt;/P&gt;&lt;P&gt;2) that you can't install the required drivers when it does?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For 1) check&lt;/P&gt;&lt;P&gt;Pull-downs on D+/-&amp;nbsp; (done)&lt;/P&gt;&lt;P&gt;Check that D+ &amp;amp; D- aren't transposed! It is surprisingly easy to do.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Crystal osc is OK (using a cro if possible), check crystal, caps &amp;amp; resistor.&lt;/P&gt;&lt;P&gt;100nF (or 470nF advice varies!)&amp;nbsp; on reset pin - seems to help with the POR&lt;/P&gt;&lt;P&gt;Filter caps on Vreg&lt;/P&gt;&lt;P&gt;Device is blank - ICP is only automatic on a blank device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For 2)&lt;/P&gt;&lt;P&gt;Are you prompted for a driver when first plugging in?&lt;/P&gt;&lt;P&gt;Check in the hardware manager under windows for the device.&amp;nbsp; If it doesn't appear at all then it's probably a hardware problem.&lt;/P&gt;&lt;P&gt;If it appears as a unknown device check the properties. It should be reported under "Device Instance Id" as&lt;/P&gt;&lt;P&gt;&amp;nbsp;USB\VID_0425&amp;amp;PID_FF02\5&amp;amp;12D03F87&amp;amp;0&amp;amp;1&lt;BR /&gt;If so, then the device is being recognized correctly and it's a driver problem.&amp;nbsp; Right-click on the device and re-install the driver from that supplied with the AN2399SW.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Not much else to check - It has worked reliably for me under windows-XP SP1, 2 &amp;amp; 3.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;hope this helps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by pgo on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-09-21&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;11:24 AM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Sep 2009 08:22:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-jb16/m-p/217264#M18926</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2009-09-21T08:22:54Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with jb16.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-jb16/m-p/217265#M18927</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks, for your help. I proved all that you tell me but I am not sure about the&lt;BR /&gt;conection D+ and D-. bye&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by nic on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-09-21&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;05:15 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Sep 2009 23:11:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Problems-with-jb16/m-p/217265#M18927</guid>
      <dc:creator>nic</dc:creator>
      <dc:date>2009-09-21T23:11:49Z</dc:date>
    </item>
  </channel>
</rss>