<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックHelp needed with RS08</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-needed-with-RS08/m-p/216834#M18865</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've suscessfully used a RS08KA4 in the past, however, that was when I was running Windows XP, CW 6.0, and with the inDart plug-in to allow direct connection to the demo08 board.&amp;nbsp; Now that I have moved to Windows 7, those tools are not available (won't install).&amp;nbsp; I've loaded CW 10.0 though 10.3 (10.3 is awful btw, full of bugs... I can give details later).&amp;nbsp; Anyway, Now I have the same micro software moved over to Windows 7 and CW 10.2.&amp;nbsp; I've added the BDM port to the demo board and removed the USB jumpers. I also have a cyclone Pro Rev B connecting the PC and the demo board. &lt;/P&gt;&lt;P&gt;When I use the full chip simulation, the software runs perfectly; which was to be expected as this software has been running for about a year now.&amp;nbsp; However, when I flash the device, CW reports back that everything flashed ok, but the chip is brain dead.&amp;nbsp; The BDM pin (Pin 2) is being forced low somehow; and this happens reqardless of the SOPT register setting (I've tried both enabling and disabling the BDM function).&amp;nbsp; All of Port B pins are high, and PTA0 -1 are forced low.&amp;nbsp; I've tried mulitple chips, and even have created my own interface board to see if that would help.&amp;nbsp; Every time CW reports back no errors and there are no error leds lit on the cyclone pro.&amp;nbsp; I've downloaded the latest programming routines from P&amp;amp;E to no avail as well.&lt;/P&gt;&lt;P&gt;Furthermore, when I try to enter debug mode (via usb to cyclone pro), I get an error along the lines of "Downloading 3rd party software....".&amp;nbsp; When I use CW 10.3, I don't even get that far, just errors out and closes the window and no error log.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I really would like to use the latest sofware and I would not want to go back to XP and CW 6.0.&amp;nbsp; I know nI can't be the only one trying to use the RS08 with the latest software.&amp;nbsp; Is is possible that the Cyclone Pro Rev B is the problem?&amp;nbsp; I did take a firmware update when I connected the first time to CW 10.2, so I assume the firmware is up to date.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry for the long post, but I wanted to give as much background / description as possible.&amp;nbsp; I hope someone can help, I've wasted two days and have ran out of options.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Dec 2012 04:18:53 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2012-12-24T04:18:53Z</dc:date>
    <item>
      <title>Help needed with RS08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-needed-with-RS08/m-p/216834#M18865</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've suscessfully used a RS08KA4 in the past, however, that was when I was running Windows XP, CW 6.0, and with the inDart plug-in to allow direct connection to the demo08 board.&amp;nbsp; Now that I have moved to Windows 7, those tools are not available (won't install).&amp;nbsp; I've loaded CW 10.0 though 10.3 (10.3 is awful btw, full of bugs... I can give details later).&amp;nbsp; Anyway, Now I have the same micro software moved over to Windows 7 and CW 10.2.&amp;nbsp; I've added the BDM port to the demo board and removed the USB jumpers. I also have a cyclone Pro Rev B connecting the PC and the demo board. &lt;/P&gt;&lt;P&gt;When I use the full chip simulation, the software runs perfectly; which was to be expected as this software has been running for about a year now.&amp;nbsp; However, when I flash the device, CW reports back that everything flashed ok, but the chip is brain dead.&amp;nbsp; The BDM pin (Pin 2) is being forced low somehow; and this happens reqardless of the SOPT register setting (I've tried both enabling and disabling the BDM function).&amp;nbsp; All of Port B pins are high, and PTA0 -1 are forced low.&amp;nbsp; I've tried mulitple chips, and even have created my own interface board to see if that would help.&amp;nbsp; Every time CW reports back no errors and there are no error leds lit on the cyclone pro.&amp;nbsp; I've downloaded the latest programming routines from P&amp;amp;E to no avail as well.&lt;/P&gt;&lt;P&gt;Furthermore, when I try to enter debug mode (via usb to cyclone pro), I get an error along the lines of "Downloading 3rd party software....".&amp;nbsp; When I use CW 10.3, I don't even get that far, just errors out and closes the window and no error log.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I really would like to use the latest sofware and I would not want to go back to XP and CW 6.0.&amp;nbsp; I know nI can't be the only one trying to use the RS08 with the latest software.&amp;nbsp; Is is possible that the Cyclone Pro Rev B is the problem?&amp;nbsp; I did take a firmware update when I connected the first time to CW 10.2, so I assume the firmware is up to date.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry for the long post, but I wanted to give as much background / description as possible.&amp;nbsp; I hope someone can help, I've wasted two days and have ran out of options.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Dec 2012 04:18:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Help-needed-with-RS08/m-p/216834#M18865</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2012-12-24T04:18:53Z</dc:date>
    </item>
  </channel>
</rss>