<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Zigbee AF_DataRequest directly from one end device to another?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Zigbee-AF-DataRequest-directly-from-one-end-device-to-another/m-p/216471#M18827</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Hello, I am trying to send a AF_DataRequest directly from one End Device to another on a small zigbee network (two end devices, one coordinator). When starting in BeeKit I specified a mesh network, however, every packet I send ends up going through the coordinator (concequently making two hops).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My question is, how can I force it to make the trip in one hop, without relaying through the coordinator?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;(if it matters, I'm using the 16 bit addressing to send the broadcast (0xFF 0xFF). Although, even if I address the end devices short address directly I get the exact same result)&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Jan 2009 22:31:22 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2009-01-15T22:31:22Z</dc:date>
    <item>
      <title>Zigbee AF_DataRequest directly from one end device to another?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Zigbee-AF-DataRequest-directly-from-one-end-device-to-another/m-p/216471#M18827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Hello, I am trying to send a AF_DataRequest directly from one End Device to another on a small zigbee network (two end devices, one coordinator). When starting in BeeKit I specified a mesh network, however, every packet I send ends up going through the coordinator (concequently making two hops).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My question is, how can I force it to make the trip in one hop, without relaying through the coordinator?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;(if it matters, I'm using the 16 bit addressing to send the broadcast (0xFF 0xFF). Although, even if I address the end devices short address directly I get the exact same result)&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jan 2009 22:31:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Zigbee-AF-DataRequest-directly-from-one-end-device-to-another/m-p/216471#M18827</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-01-15T22:31:22Z</dc:date>
    </item>
    <item>
      <title>Re: Zigbee AF_DataRequest directly from one end device to another?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Zigbee-AF-DataRequest-directly-from-one-end-device-to-another/m-p/216472#M18828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Tecmec,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;This is NOT possible. An End Device is a Reduced functionality device (look in 802.15.4 spec for more info) It ONLY has the capability to communicate to its parent. the Parent must handle the routing.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;A Router or coordinator can communicate directly to another device within its hearing range, if it creates a mesh route first.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Using a broadcast address will make the End device send a packet to its parent, which then will handle the broadcasting to the rest of the network.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;BR,&lt;/DIV&gt;&lt;DIV&gt;Mads&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jan 2009 17:45:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Zigbee-AF-DataRequest-directly-from-one-end-device-to-another/m-p/216472#M18828</guid>
      <dc:creator>Mads</dc:creator>
      <dc:date>2009-01-16T17:45:45Z</dc:date>
    </item>
  </channel>
</rss>