<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックMC9S08LL16 GPIO shareed with LCD pins  problem</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LL16-GPIO-shareed-with-LCD-pins-problem/m-p/215350#M18665</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am using MC9s08LL16. I find&amp;nbsp;PTD and PTE which are shared with LCD pins only output&amp;nbsp;3V. However I have disable the LCD&amp;nbsp;module as I&amp;nbsp;only use them as GPIO to output 3.3V logic level.&amp;nbsp;Here is the codes:&lt;/P&gt;&lt;P&gt;&amp;nbsp; LCDSUPPLY_CPSEL = 1;&lt;BR /&gt;&amp;nbsp; LCDSUPPLY_LADJ = 0;&lt;BR /&gt;&amp;nbsp; LCDSUPPLY_BBYPASS = 0;&lt;BR /&gt;&amp;nbsp; LCDSUPPLY_VSUPPLY1 = 0;&lt;BR /&gt;&amp;nbsp; LCDSUPPLY_VSUPPLY0 = 1;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; LCDC0_LCDEN = 0;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; LCDC1_FCDEN = 1;&lt;BR /&gt;&amp;nbsp; LCDRVC_RVEN = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone helps me? Thanks a lot!&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif"&gt;&lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Jul 2010 20:31:09 GMT</pubDate>
    <dc:creator>VincentLau</dc:creator>
    <dc:date>2010-07-28T20:31:09Z</dc:date>
    <item>
      <title>MC9S08LL16 GPIO shareed with LCD pins  problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LL16-GPIO-shareed-with-LCD-pins-problem/m-p/215350#M18665</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am using MC9s08LL16. I find&amp;nbsp;PTD and PTE which are shared with LCD pins only output&amp;nbsp;3V. However I have disable the LCD&amp;nbsp;module as I&amp;nbsp;only use them as GPIO to output 3.3V logic level.&amp;nbsp;Here is the codes:&lt;/P&gt;&lt;P&gt;&amp;nbsp; LCDSUPPLY_CPSEL = 1;&lt;BR /&gt;&amp;nbsp; LCDSUPPLY_LADJ = 0;&lt;BR /&gt;&amp;nbsp; LCDSUPPLY_BBYPASS = 0;&lt;BR /&gt;&amp;nbsp; LCDSUPPLY_VSUPPLY1 = 0;&lt;BR /&gt;&amp;nbsp; LCDSUPPLY_VSUPPLY0 = 1;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; LCDC0_LCDEN = 0;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; LCDC1_FCDEN = 1;&lt;BR /&gt;&amp;nbsp; LCDRVC_RVEN = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone helps me? Thanks a lot!&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif"&gt;&lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jul 2010 20:31:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LL16-GPIO-shareed-with-LCD-pins-problem/m-p/215350#M18665</guid>
      <dc:creator>VincentLau</dc:creator>
      <dc:date>2010-07-28T20:31:09Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08LL16 GPIO shareed with LCD pins  problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LL16-GPIO-shareed-with-LCD-pins-problem/m-p/215351#M18666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vincent,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know very little about this, but do remember that similar issues have been discussed here before.&lt;/P&gt;&lt;P&gt;Have you searched here?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jul 2010 04:36:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08LL16-GPIO-shareed-with-LCD-pins-problem/m-p/215351#M18666</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2010-07-29T04:36:19Z</dc:date>
    </item>
  </channel>
</rss>