<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 TPM</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM/m-p/214746#M18601</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm trying to set up the S08TPMV3 module in MC9S08DZ32 for the first time and some questions arises.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm planning to use TPM2 as a pure SW timer and in the Data Sheet for MC9S08DZ32, chapter 16.1.2 (Modes of operation) it's written:&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="color: #66CC33;"&gt;The output compare action may be selected to force the pin to zero, force the pin to one, toggle the pin, or&lt;/SPAN&gt; &lt;SPAN style="color: #FF3300;"&gt;ignore the pin&lt;/SPAN&gt; &lt;SPAN style="color: #ff0000;"&gt;(used for software timing functions).&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Then I read the register definitions under 16.3.4 and in the table 16-6 all configurations for the output compare mode are mentioned except for the 'ignore pin mode'. The ELSnB:ELSnA combination 0:0 is omitted in the table and I wonder if this might be the setting for the 'ignore pin mode'.?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Is it possible to use the TPM as a software timer, ignore the pin and then use this pin for general I/O purposes at the same time??&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;Bengt-Olov&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Jan 2009 23:03:02 GMT</pubDate>
    <dc:creator>BAN</dc:creator>
    <dc:date>2009-01-09T23:03:02Z</dc:date>
    <item>
      <title>TPM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM/m-p/214746#M18601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm trying to set up the S08TPMV3 module in MC9S08DZ32 for the first time and some questions arises.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm planning to use TPM2 as a pure SW timer and in the Data Sheet for MC9S08DZ32, chapter 16.1.2 (Modes of operation) it's written:&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN style="color: #66CC33;"&gt;The output compare action may be selected to force the pin to zero, force the pin to one, toggle the pin, or&lt;/SPAN&gt; &lt;SPAN style="color: #FF3300;"&gt;ignore the pin&lt;/SPAN&gt; &lt;SPAN style="color: #ff0000;"&gt;(used for software timing functions).&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Then I read the register definitions under 16.3.4 and in the table 16-6 all configurations for the output compare mode are mentioned except for the 'ignore pin mode'. The ELSnB:ELSnA combination 0:0 is omitted in the table and I wonder if this might be the setting for the 'ignore pin mode'.?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Is it possible to use the TPM as a software timer, ignore the pin and then use this pin for general I/O purposes at the same time??&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards&lt;/DIV&gt;&lt;DIV&gt;Bengt-Olov&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jan 2009 23:03:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM/m-p/214746#M18601</guid>
      <dc:creator>BAN</dc:creator>
      <dc:date>2009-01-09T23:03:02Z</dc:date>
    </item>
    <item>
      <title>Re: TPM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM/m-p/214747#M18602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello BAN,&lt;BR /&gt;&lt;BR /&gt;In the manual I'm looking at (Rev.4 6/2008) Table 16-6 is split over a page break.&lt;BR /&gt;The description for ELSnB:ELSnA = 00 is on the previous page to the rest of the table.&lt;BR /&gt;It works as always to effectively free the pin for other uses.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 10 Jan 2009 04:35:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM/m-p/214747#M18602</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2009-01-10T04:35:27Z</dc:date>
    </item>
    <item>
      <title>Re: TPM</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM/m-p/214748#M18603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello Bengt-Olov,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;As Peg said the pin is used for normal General purpose I/O.No where related to TPM/Output compare.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;BLOCKQUOTE&gt;&lt;DIV&gt;&lt;HR /&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Is it possible to use the TPM as a software timer, ignore the pin and then use this pin for general I/O purposes at the same time??&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;DIV&gt;I would say yes.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Also note: S08TPM version 3, which applies to the 0M74K and newer mask sets of this device. 3M05C and older ask set devices use S08TPM version 2.One cannot randomly use it .&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jan 2009 21:29:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TPM/m-p/214748#M18603</guid>
      <dc:creator>denny_george</dc:creator>
      <dc:date>2009-01-15T21:29:47Z</dc:date>
    </item>
  </channel>
</rss>