<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Simple usb dll and VS in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Simple-usb-dll-and-VS/m-p/214342#M18547</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I have read it&lt;/P&gt;&lt;P&gt;im using C++ now C#&lt;/P&gt;&lt;P&gt;and I couldn t get it to compile&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But now it work (have tried a device yet)&lt;/P&gt;&lt;P&gt;had to run vs in admin to add the simple usb dll component then i could use it as a user&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Jun 2011 21:05:10 GMT</pubDate>
    <dc:creator>Juls</dc:creator>
    <dc:date>2011-06-13T21:05:10Z</dc:date>
    <item>
      <title>Simple usb dll and VS</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Simple-usb-dll-and-VS/m-p/214340#M18545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I have made a cdc device work well&lt;/P&gt;&lt;P&gt;but not its time to move to completly usb&lt;/P&gt;&lt;P&gt;Im using a JM60 and im under windows 7 X64 and vs2010&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did listen to How to make a graphical user interface (GUI) for USB communication training twice&lt;/P&gt;&lt;P&gt;My vs project is in CLR (way more easier to build gui)&lt;/P&gt;&lt;P&gt;and at the part to drag the dll into the tool box I get a bug&lt;/P&gt;&lt;P&gt;placing it work but trying to place the simple usb into my form throw and error about LFSwinusb.dll in vs install directory (that file doesnt exist. and the object is not created &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-frustrated.gif"&gt;&lt;IMG alt=":smileyfrustrated:" class="emoticon emoticon-smileyfrustrated" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-frustrated.gif" title="Smiley Frustrated" /&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyone made that work?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ive also spend 2-3 hours trying to make winusb work but im not able to make all that compile&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jun 2011 05:51:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Simple-usb-dll-and-VS/m-p/214340#M18545</guid>
      <dc:creator>Juls</dc:creator>
      <dc:date>2011-06-13T05:51:32Z</dc:date>
    </item>
    <item>
      <title>Re: Simple usb dll and VS</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Simple-usb-dll-and-VS/m-p/214341#M18546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In this topic, it was discussed once.&lt;BR /&gt;&lt;BR /&gt;SimpleUSB &amp;amp; Windows 7&lt;BR /&gt;&lt;A __default_attr="80364" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/80364" jivemacro="thread" title="https://community.freescale.com/thread/80364"&gt;https://community.freescale.com/thread/80364&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Tsuneo﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jun 2011 09:54:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Simple-usb-dll-and-VS/m-p/214341#M18546</guid>
      <dc:creator>Tsuneo</dc:creator>
      <dc:date>2011-06-13T09:54:41Z</dc:date>
    </item>
    <item>
      <title>Re: Simple usb dll and VS</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Simple-usb-dll-and-VS/m-p/214342#M18547</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I have read it&lt;/P&gt;&lt;P&gt;im using C++ now C#&lt;/P&gt;&lt;P&gt;and I couldn t get it to compile&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But now it work (have tried a device yet)&lt;/P&gt;&lt;P&gt;had to run vs in admin to add the simple usb dll component then i could use it as a user&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jun 2011 21:05:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Simple-usb-dll-and-VS/m-p/214342#M18547</guid>
      <dc:creator>Juls</dc:creator>
      <dc:date>2011-06-13T21:05:10Z</dc:date>
    </item>
  </channel>
</rss>