<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: Using 08jm processor and usb with uarts</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-08jm-processor-and-usb-with-uarts/m-p/213432#M18401</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My understanding is that, for USB operation, a bus clock of 24 MHz is required, generated using PEE mode.&amp;nbsp; You do not mention the SCI baud rate that you require, but it should be possible to generate a range of standard baud rates with this high bus frequency.&amp;nbsp; For example, a baud divisor of 13 would generate 115,200 bit per second, and a baud rate divisor of 78 would generate 19,200 bit per second.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Sep 2009 21:14:26 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2009-09-02T21:14:26Z</dc:date>
    <item>
      <title>Using 08jm processor and usb with uarts</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-08jm-processor-and-usb-with-uarts/m-p/213431#M18400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks in advance for your thoughts&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;11.0592 for the uarts or the specified multiple oe 2mhz &amp;nbsp;for the usb which would take me to 12mhz...&lt;/P&gt;&lt;P&gt;so then my question is what xtal ( crystal ) do i use.... 11.0592 &amp;nbsp;or 12mhz...&lt;/P&gt;&lt;P&gt;i have a problem that im going to use the usb port for boot loading and gtghe uarts for rs232 comms&lt;/P&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2009 09:48:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-08jm-processor-and-usb-with-uarts/m-p/213431#M18400</guid>
      <dc:creator>Danzo</dc:creator>
      <dc:date>2009-09-02T09:48:01Z</dc:date>
    </item>
    <item>
      <title>Re: Using 08jm processor and usb with uarts</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-08jm-processor-and-usb-with-uarts/m-p/213432#M18401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My understanding is that, for USB operation, a bus clock of 24 MHz is required, generated using PEE mode.&amp;nbsp; You do not mention the SCI baud rate that you require, but it should be possible to generate a range of standard baud rates with this high bus frequency.&amp;nbsp; For example, a baud divisor of 13 would generate 115,200 bit per second, and a baud rate divisor of 78 would generate 19,200 bit per second.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2009 21:14:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-08jm-processor-and-usb-with-uarts/m-p/213432#M18401</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2009-09-02T21:14:26Z</dc:date>
    </item>
  </channel>
</rss>