<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: MC9S08 in stop mode</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08-in-stop-mode/m-p/213099#M18382</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;See this &lt;A href="https://community.freescale.com/message/96506#96506" title="https://community.freescale.com/message/96506#96506"&gt;https://community.freescale.com/message/96506#96506&lt;/A&gt;. Make sure you are turning off ICSIRCLK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As an aside, every input pin should be at ground or vcc of the chip. Every output pin should not be loaded.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did you disable all your peripherals and and THEN shut the clocks off to them?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Mar 2012 04:34:16 GMT</pubDate>
    <dc:creator>PG1</dc:creator>
    <dc:date>2012-03-07T04:34:16Z</dc:date>
    <item>
      <title>MC9S08 in stop mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08-in-stop-mode/m-p/213098#M18381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;BR /&gt;i'm programming a mc9s08qe8 with codewarrior.&lt;BR /&gt;i use device initialization to configure the chip.&lt;BR /&gt;i'm working with 1MHz bus clock in FEI mode. i've all periperals disabled.&lt;BR /&gt;i've enable "stop instruction enabled".&lt;BR /&gt;i'd like to put the uC in stop3 mode, in the main there is "asm STOP;".&lt;BR /&gt;it goes in stop but the uC absorbs 40uA insted of 1uA...&lt;BR /&gt;i don't know how i can reduce the current... i think there is something that i've to switch off!&lt;BR /&gt;someone can help me?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Mar 2012 18:45:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08-in-stop-mode/m-p/213098#M18381</guid>
      <dc:creator>Enry86cami</dc:creator>
      <dc:date>2012-03-06T18:45:57Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08 in stop mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08-in-stop-mode/m-p/213099#M18382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;See this &lt;A href="https://community.freescale.com/message/96506#96506" title="https://community.freescale.com/message/96506#96506"&gt;https://community.freescale.com/message/96506#96506&lt;/A&gt;. Make sure you are turning off ICSIRCLK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As an aside, every input pin should be at ground or vcc of the chip. Every output pin should not be loaded.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did you disable all your peripherals and and THEN shut the clocks off to them?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Mar 2012 04:34:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08-in-stop-mode/m-p/213099#M18382</guid>
      <dc:creator>PG1</dc:creator>
      <dc:date>2012-03-07T04:34:16Z</dc:date>
    </item>
  </channel>
</rss>