<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using demo boards as BDM interfaces in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-demo-boards-as-BDM-interfaces-08AW60/m-p/212362#M18324</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;In all cases I am using 5 volts.&amp;nbsp; I have tried using the USB from my host PC, and using the target power.&lt;BR /&gt;&lt;BR /&gt;Oddly (or perhaps by design)&amp;nbsp; the exact same setup works fine with CW 6.1&amp;nbsp; no problems.&amp;nbsp; When I use CW 6.2, the true-time application cannot enter background mode.&lt;BR /&gt;&lt;BR /&gt;Bob&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Dec 2008 17:44:28 GMT</pubDate>
    <dc:creator>TurboBob</dc:creator>
    <dc:date>2008-12-24T17:44:28Z</dc:date>
    <item>
      <title>Using demo boards as BDM interfaces - 08AW60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-demo-boards-as-BDM-interfaces-08AW60/m-p/212360#M18322</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;A little background:&amp;nbsp; I have been using CW6.1 for a while with the AW60 demo board to develop my JM60 application.&amp;nbsp; It seems to work ok, but I am suspecting a bug in 6.1 and tried to update to 6.2&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;My CW installation is fully licensed.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;When updating to 6.2, the AW60 demo board&amp;nbsp;was not accepted by the TrueTime app as a valid interface for a JM60 chip.&amp;nbsp; Since I have almost all of the demo kits, I got out my JM demo kit, put a header on it and plugged it in.&amp;nbsp; TrueTime updated the&amp;nbsp;firmware, and appears willing to talk to it.&amp;nbsp; It will load my code into an on-board JM60 chip,&amp;nbsp; but it will not connect to my target (remove daughter card, plug in ribbon cable).&amp;nbsp; It does halt the target system but will not connect.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The demoboard will connect,load, and run if I use the CW6.1 to connect to it (yes I have 6.1 and 6.2 loaded on my machine.)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I hope I am being clear,&amp;nbsp; basically 6.2 won't talk to my target, but will talk to a chip on the demo board.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Any ideas?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Bob Bailey&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Added p/n to subject.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by NLFSJ on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2008-12-24&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;07:19 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Dec 2008 16:11:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-demo-boards-as-BDM-interfaces-08AW60/m-p/212360#M18322</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2008-12-24T16:11:55Z</dc:date>
    </item>
    <item>
      <title>Re: Using demo boards as BDM interfaces</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-demo-boards-as-BDM-interfaces-08AW60/m-p/212361#M18323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;On AW60 board, is your chip supplied with&amp;nbsp;5V or 3.3V? Is chip on your target board&amp;nbsp;powered the same? I don't know, but I guess that BDM on demo board may lack voltage level translator like in full featured USB-ML-12.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Dec 2008 17:02:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-demo-boards-as-BDM-interfaces-08AW60/m-p/212361#M18323</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2008-12-24T17:02:23Z</dc:date>
    </item>
    <item>
      <title>Re: Using demo boards as BDM interfaces</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-demo-boards-as-BDM-interfaces-08AW60/m-p/212362#M18324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;In all cases I am using 5 volts.&amp;nbsp; I have tried using the USB from my host PC, and using the target power.&lt;BR /&gt;&lt;BR /&gt;Oddly (or perhaps by design)&amp;nbsp; the exact same setup works fine with CW 6.1&amp;nbsp; no problems.&amp;nbsp; When I use CW 6.2, the true-time application cannot enter background mode.&lt;BR /&gt;&lt;BR /&gt;Bob&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Dec 2008 17:44:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-demo-boards-as-BDM-interfaces-08AW60/m-p/212362#M18324</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2008-12-24T17:44:28Z</dc:date>
    </item>
    <item>
      <title>Re: Using demo boards as BDM interfaces</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-demo-boards-as-BDM-interfaces-08AW60/m-p/212363#M18325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Oh, on QE (and JM probably)&amp;nbsp;/RESET pin by default is not functioning as /RESET, but as I/O pin. To enter special mode, target should be reset with BKGD pulled low. Since there's no real /RESET pin, external reset can be done&amp;nbsp;only cycling target power&amp;nbsp;on/off. Isn't demo board cycling socket power on/off?&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;Message Edited by kef on &lt;SPAN class="date_text"&gt;2008-12-24&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;12:36 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Dec 2008 18:33:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Using-demo-boards-as-BDM-interfaces-08AW60/m-p/212363#M18325</guid>
      <dc:creator>kef</dc:creator>
      <dc:date>2008-12-24T18:33:47Z</dc:date>
    </item>
  </channel>
</rss>