<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックBluetooth with JM60 via Serial Port</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bluetooth-with-JM60-via-Serial-Port/m-p/211932#M18268</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Folks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working on a project that we want to be using BT to communicate&lt;/P&gt;&lt;P&gt;with a host PC or WinCE device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The BT module I'm looking at is the Panasonic PAN1321, which uses&lt;/P&gt;&lt;P&gt;'AT' commands to communicate via a serial port.&amp;nbsp; Also seems to be&lt;/P&gt;&lt;P&gt;pretty cost effective for volume production.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, just knowing how things in the PC world aren't&amp;nbsp;easily portable&lt;/P&gt;&lt;P&gt;back to our microcontrollers, will I need extensive Stack software to&lt;/P&gt;&lt;P&gt;provide connectivity with an external computer?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I see that Microchip has a stack for their micros... wondering if there is&lt;/P&gt;&lt;P&gt;one that the 08 family could make use of.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Something tells me that it's not going to be as easy to talk to as an old&lt;/P&gt;&lt;P&gt;Hayes modem with AT commands!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 05 Jun 2011 03:50:01 GMT</pubDate>
    <dc:creator>UtopiaTim</dc:creator>
    <dc:date>2011-06-05T03:50:01Z</dc:date>
    <item>
      <title>Bluetooth with JM60 via Serial Port</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bluetooth-with-JM60-via-Serial-Port/m-p/211932#M18268</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Folks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working on a project that we want to be using BT to communicate&lt;/P&gt;&lt;P&gt;with a host PC or WinCE device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The BT module I'm looking at is the Panasonic PAN1321, which uses&lt;/P&gt;&lt;P&gt;'AT' commands to communicate via a serial port.&amp;nbsp; Also seems to be&lt;/P&gt;&lt;P&gt;pretty cost effective for volume production.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, just knowing how things in the PC world aren't&amp;nbsp;easily portable&lt;/P&gt;&lt;P&gt;back to our microcontrollers, will I need extensive Stack software to&lt;/P&gt;&lt;P&gt;provide connectivity with an external computer?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I see that Microchip has a stack for their micros... wondering if there is&lt;/P&gt;&lt;P&gt;one that the 08 family could make use of.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Something tells me that it's not going to be as easy to talk to as an old&lt;/P&gt;&lt;P&gt;Hayes modem with AT commands!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Jun 2011 03:50:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Bluetooth-with-JM60-via-Serial-Port/m-p/211932#M18268</guid>
      <dc:creator>UtopiaTim</dc:creator>
      <dc:date>2011-06-05T03:50:01Z</dc:date>
    </item>
    <item>
      <title>Re: Bluetooth with JM60 via Serial Port</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bluetooth-with-JM60-via-Serial-Port/m-p/211933#M18269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you are looking to connect as a BT serial device, I have been using this:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.mdfly.com/index.php?main_page=product_info&amp;amp;cPath=8_47&amp;amp;products_id=769" rel="nofollow" target="_blank"&gt;MDFly Bluetooth&lt;/A&gt;&lt;/P&gt;&lt;P&gt;All you do is connect from the PC (or, in my case Android) and it the serial port on the MCU is connected no fuss no muss.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Jun 2011 09:26:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Bluetooth-with-JM60-via-Serial-Port/m-p/211933#M18269</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2011-06-05T09:26:34Z</dc:date>
    </item>
  </channel>
</rss>