<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: microcontroller to microcontroller communication</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/microcontroller-to-microcontroller-communication/m-p/210048#M17970</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;- Do you get any receive flags at all set in the S08? Such as framing error, overrun error etc? If not, they aren't connected properly. Measure on Rx pin with an oscilloscope. Or perhaps the debugger is destroying the "clear-by-reading" flag registers. Run the program without debugger connected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Any buffers etc between the MCUs? Are both MCUs running at the same voltage?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Less likely: missing pull-up on RX line. PIC clock being too inacurrate, yielding a baudrate fault larger than 3%. In these cases you should at least get framing errors etc.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Btw is there any particular reason why you would use a MAX232 in new designs? Why not use an alternative without the huge caps, like MAX202?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Jul 2010 20:20:04 GMT</pubDate>
    <dc:creator>Lundin</dc:creator>
    <dc:date>2010-07-01T20:20:04Z</dc:date>
    <item>
      <title>microcontroller to microcontroller communication</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/microcontroller-to-microcontroller-communication/m-p/210047#M17969</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;dear sir/madam;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i had communicated Freescale MC9S08AW60 to PCsuccessfully &amp;nbsp;but&amp;nbsp;in second application&amp;nbsp; unable to communicate with microcontroller PIC 18f452&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In this application&lt;/P&gt;&lt;P&gt;Mc9s08AW60 is unable &amp;nbsp;to get data from microchip PIC 18f452 where as it is able to send data to PIC 18f452&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Points already covered by me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1.&amp;gt; Software is same which is communicating &amp;nbsp;from PC. ( hence all setting are same as well as all initialisation what we are using in PC communication&amp;nbsp;)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2.&amp;gt; IC MAX232 ( In case of PC communication ) is removed and RX and TX are connected to each other.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;3.&amp;gt; Transmission had gone through properly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;4.&amp;gt; unable to get data from&amp;nbsp;microcontroller.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I request a fast feedback .it will be highly appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR&lt;BR /&gt;Hasan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Jul 2010 18:17:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/microcontroller-to-microcontroller-communication/m-p/210047#M17969</guid>
      <dc:creator>avl</dc:creator>
      <dc:date>2010-07-01T18:17:57Z</dc:date>
    </item>
    <item>
      <title>Re: microcontroller to microcontroller communication</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/microcontroller-to-microcontroller-communication/m-p/210048#M17970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;- Do you get any receive flags at all set in the S08? Such as framing error, overrun error etc? If not, they aren't connected properly. Measure on Rx pin with an oscilloscope. Or perhaps the debugger is destroying the "clear-by-reading" flag registers. Run the program without debugger connected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Any buffers etc between the MCUs? Are both MCUs running at the same voltage?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Less likely: missing pull-up on RX line. PIC clock being too inacurrate, yielding a baudrate fault larger than 3%. In these cases you should at least get framing errors etc.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Btw is there any particular reason why you would use a MAX232 in new designs? Why not use an alternative without the huge caps, like MAX202?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Jul 2010 20:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/microcontroller-to-microcontroller-communication/m-p/210048#M17970</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2010-07-01T20:20:04Z</dc:date>
    </item>
  </channel>
</rss>