<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: S08QE8 Background Debug Mode</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-Background-Debug-Mode/m-p/209880#M17933</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;I&gt;&lt;B&gt;I used an external power to supply MCU but i connect GND of MCU to Pin 2 of BDM connector&lt;/B&gt;&lt;/I&gt;&lt;BR /&gt;&lt;BR /&gt;It might just be the way you phrased it but, you do have your external power supply's ground connected as well don't you?&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Dec 2008 09:40:25 GMT</pubDate>
    <dc:creator>alexod</dc:creator>
    <dc:date>2008-12-23T09:40:25Z</dc:date>
    <item>
      <title>S08QE8 Background Debug Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-Background-Debug-Mode/m-p/209878#M17931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I try to program my MCU S08QE8 with cyclone pro but i have error message when i try to connect emulator to MCU&lt;BR /&gt;Loading Target ...&lt;BR /&gt;Windows NT detected.&lt;BR /&gt;CYCLONE PRO detected - Flash Version 8.09&lt;BR /&gt;Frequency change to ~0hz.&lt;BR /&gt;Frequency change to ~0hz.&lt;BR /&gt;CYCLONE PRO detected - Flash Version 8.09&lt;BR /&gt;Frequency change to ~0hz.&lt;BR /&gt;Frequency change to ~0hz.&lt;BR /&gt;Frequency change to ~0hz.&lt;BR /&gt;Frequency change to ~0hz.&lt;BR /&gt;Frequency change to ~0hz.&lt;BR /&gt;Frequency change to ~8032hz.&lt;BR /&gt;&lt;BR /&gt;Error: Can not enter background mode.&lt;BR /&gt;&lt;BR /&gt;I check my RESET (Pin 1 of MCU) and BKGD (pin 2 of MCU) signals&lt;BR /&gt;On Pin 1 i have 0.4V i thonk OK to do reset.&lt;BR /&gt;On pin 2, i have 0.7V!!!&lt;BR /&gt;In fact i directly connect PIN 1 of BDM connector from Cyclone to Pin 2 of MCU. Is it correct?&lt;BR /&gt;I used an external power to supply MCU but i connect GND of MCU to Pin 2 of BDM connector&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Somebody ou somewhere can i find some descriptions, explanation about connections between cyclone emulator and MCU S08QE8?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;thanks&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;David&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Dec 2008 15:55:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-Background-Debug-Mode/m-p/209878#M17931</guid>
      <dc:creator>DavidoBG</dc:creator>
      <dc:date>2008-12-15T15:55:46Z</dc:date>
    </item>
    <item>
      <title>Re: S08QE8 Background Debug Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-Background-Debug-Mode/m-p/209879#M17932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Dear Davido,&lt;BR /&gt;&lt;BR /&gt;BDM physical interface is quite simple, it uses mainly BKGD.&lt;BR /&gt;In order to enter BKGD mode you have to have BKGD in 0V and reset the uC.&lt;BR /&gt;The problem is that sometimes reset pin is not programmed as that.&lt;BR /&gt;The only way to assure this is thru pwr-up reset.&lt;BR /&gt;&lt;BR /&gt;Suggestion from someone who has burned more than 8 EVB BDMs: use 0.1A PPTCs in series with GND(2), BKGD(1), RST(4) and VDD(6 - if you use it). Pullups to VDD&amp;nbsp; from RST and BKGD are nice too.&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;&lt;BR /&gt;Celso&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Dec 2008 21:20:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-Background-Debug-Mode/m-p/209879#M17932</guid>
      <dc:creator>celsoken</dc:creator>
      <dc:date>2008-12-15T21:20:03Z</dc:date>
    </item>
    <item>
      <title>Re: S08QE8 Background Debug Mode</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-Background-Debug-Mode/m-p/209880#M17933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;I&gt;&lt;B&gt;I used an external power to supply MCU but i connect GND of MCU to Pin 2 of BDM connector&lt;/B&gt;&lt;/I&gt;&lt;BR /&gt;&lt;BR /&gt;It might just be the way you phrased it but, you do have your external power supply's ground connected as well don't you?&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Dec 2008 09:40:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08QE8-Background-Debug-Mode/m-p/209880#M17933</guid>
      <dc:creator>alexod</dc:creator>
      <dc:date>2008-12-23T09:40:25Z</dc:date>
    </item>
  </channel>
</rss>