<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: HCS08 Assembler Warning A13003 - Value is truncated to one byte. in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209485#M17886</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello BarryP,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the separate&amp;nbsp;file where the variables are defined, do you XDEF each variable name?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Jun 2010 22:48:32 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2010-06-28T22:48:32Z</dc:date>
    <item>
      <title>HCS08 Assembler Warning A13003 - Value is truncated to one byte.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209484#M17885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am writing asssembly code for the HCS08SH8 and get the A13003 warning for bytes declared in SECTION RAM&amp;nbsp; in main.asm and used there and elsewhere. The vars are in zero page but the assembler doesn't seem to know this yet since it doesn't see the .prm file (where the SECTIONs are defined) until link time. I have worked around this by declaring the variables in another file and use xref.b (import reference to an external symbol located on the direct page) where they are used. Now the warnings are gone.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The problem with this is now I can't see these variables (data) in the IDE during debug since they appear to be out of the scope of the module I am debugging. Any ideas how to keep the declarations in main.asm and not get the warnings. I can always disable the A13003 warning in "options" but I would rather not do that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jun 2010 21:26:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209484#M17885</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2010-06-28T21:26:10Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 Assembler Warning A13003 - Value is truncated to one byte.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209485#M17886</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello BarryP,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the separate&amp;nbsp;file where the variables are defined, do you XDEF each variable name?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jun 2010 22:48:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209485#M17886</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-06-28T22:48:32Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 Assembler Warning A13003 - Value is truncated to one byte.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209486#M17887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Yes, I do.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jun 2010 22:49:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209486#M17887</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2010-06-28T22:49:40Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 Assembler Warning A13003 - Value is truncated to one byte.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209487#M17888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I placed a dummy subroutine (nop's) in the seperate data file so I can call it during debug. I am able to see all of the globals there in the "data" window of the debugger when I call the dummy sub. This is painful, however...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jun 2010 22:53:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209487#M17888</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2010-06-28T22:53:13Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 Assembler Warning A13003 - Value is truncated to one byte.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209488#M17889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Barry P,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am guessing here, but something else to try would be to INCLUDE the variable file ahead of the code where the variables are used.&amp;nbsp; However, you would need to add directives to the variable file to prevent multiple inclusions,&lt;/P&gt;&lt;P&gt;&amp;nbsp; IFNDEF&amp;nbsp; MY_VARIABLES&lt;/P&gt;&lt;P&gt;&amp;nbsp; DEFINE&amp;nbsp; MY_VARIABLES&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;; Define variables here&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; ENDIF&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jun 2010 23:16:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209488#M17889</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-06-28T23:16:38Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 Assembler Warning A13003 - Value is truncated to one byte.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209489#M17890</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It appears that "DEFINE" isn't a directive in the HCS08 assembler. I was able to accomplish this with:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;IFNDEF&amp;nbsp; MY_VARIABLES&lt;/P&gt;&amp;nbsp;&lt;P&gt;; Define variables here&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; ENDIF&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It appears to be working but I get the same warning, A13003.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the advice anyway.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any other options would be appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Barry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jun 2010 01:14:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209489#M17890</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2010-06-29T01:14:52Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 Assembler Warning A13003 - Value is truncated to one byte.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209490#M17891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/10929#10929" title="https://community.freescale.com/message/10929#10929"&gt;https://community.freescale.com/message/10929#10929&lt;/A&gt; deals with the two main reasons for this warning.&lt;/P&gt;&lt;P&gt;See if it helps you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jun 2010 05:05:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209490#M17891</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2010-06-29T05:05:58Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 Assembler Warning A13003 - Value is truncated to one byte.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209491#M17892</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As mentioned in thread Peg linked to relocatable sections which are intended to be allocated in the zero page should use the SHORT qualifier.&lt;/P&gt;&lt;P&gt;E.g.&lt;/P&gt;&lt;P&gt;MySectionName: Section SHORT&lt;/P&gt;&lt;P&gt;MyName: DS.B 1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jun 2010 09:37:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209491#M17892</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2010-06-29T09:37:27Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 Assembler Warning A13003 - Value is truncated to one byte.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209492#M17893</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Barry,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry about my confusion.&amp;nbsp; The conditional assembly within the include should be:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;&amp;nbsp; IFNDEF&amp;nbsp; MY_VARIABLES&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;MY_VARIABLES:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;; Define variables here&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;&amp;nbsp; ENDIF&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you did not already use the SHORT qualifier, as suggested by Compiler Guru, I suspect this will solve the warning message issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jun 2010 10:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209492#M17893</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-06-29T10:00:47Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 Assembler Warning A13003 - Value is truncated to one byte.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209493#M17894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you all for the input! I was able to rid myself of the warning by a combination of suggestions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Use of the SHORT directive for variables in the file where direct addressing is to be used with them.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Use of XDEF.B for variables declared in the file where SHORT was used that are to be referenced in other files where direct addressing is to be used.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Use of XREF.B for variables declared in the file where SHORT was used and where direct addressing is to be used.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jun 2010 23:49:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-Assembler-Warning-A13003-Value-is-truncated-to-one-byte/m-p/209493#M17894</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2010-06-29T23:49:08Z</dc:date>
    </item>
  </channel>
</rss>