<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: My 12LED charlieplexing on a RS08KA in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/My-12LED-charlieplexing-on-a-RS08KA/m-p/208642#M17764</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi to all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Before thi topic, I didn't know anything about «charlieplexing».&lt;/P&gt;&lt;P&gt;It is very&amp;nbsp;&amp;nbsp;interesting.&lt;/P&gt;&lt;P&gt;I've found on the net a scheme to use this technique also for keyboard. (see the image attached).&amp;nbsp;But I guess it isn't possible to use it with KBI to wake up the microcontroller.&lt;/P&gt;&lt;P&gt;It is true?&amp;nbsp;I've few pins free&amp;nbsp;and I need also a keyboard.. with this pin's arrangement&amp;nbsp; could I realize it (with KBI wake-up?)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Jul 2010 18:54:40 GMT</pubDate>
    <dc:creator>roberto_m</dc:creator>
    <dc:date>2010-07-09T18:54:40Z</dc:date>
    <item>
      <title>My 12LED charlieplexing on a RS08KA</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/My-12LED-charlieplexing-on-a-RS08KA/m-p/208640#M17762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Only had the RS08 protoboard for a week and this is my first project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Uses only 4pins, no additonal shiftregister&amp;nbsp;IC's&amp;nbsp;etc&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So far only have 3 animations made.&lt;/P&gt;&lt;P&gt;Each animiation&amp;nbsp;uses between 16-to 64bytes.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.youtube.com%2Fwatch%3Fv%3D8apRaZQbv5w" rel="nofollow" target="_blank"&gt;Video on youtube&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jun 2010 07:14:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/My-12LED-charlieplexing-on-a-RS08KA/m-p/208640#M17762</guid>
      <dc:creator>tonysofla</dc:creator>
      <dc:date>2010-06-23T07:14:28Z</dc:date>
    </item>
    <item>
      <title>Re: My 12LED charlieplexing on a RS08KA</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/My-12LED-charlieplexing-on-a-RS08KA/m-p/208641#M17763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nice. you can't go wrong with blue LEDs and the Knight Rider theme.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jun 2010 21:33:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/My-12LED-charlieplexing-on-a-RS08KA/m-p/208641#M17763</guid>
      <dc:creator>ThaManJD</dc:creator>
      <dc:date>2010-06-23T21:33:34Z</dc:date>
    </item>
    <item>
      <title>Re: My 12LED charlieplexing on a RS08KA</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/My-12LED-charlieplexing-on-a-RS08KA/m-p/208642#M17764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi to all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Before thi topic, I didn't know anything about «charlieplexing».&lt;/P&gt;&lt;P&gt;It is very&amp;nbsp;&amp;nbsp;interesting.&lt;/P&gt;&lt;P&gt;I've found on the net a scheme to use this technique also for keyboard. (see the image attached).&amp;nbsp;But I guess it isn't possible to use it with KBI to wake up the microcontroller.&lt;/P&gt;&lt;P&gt;It is true?&amp;nbsp;I've few pins free&amp;nbsp;and I need also a keyboard.. with this pin's arrangement&amp;nbsp; could I realize it (with KBI wake-up?)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jul 2010 18:54:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/My-12LED-charlieplexing-on-a-RS08KA/m-p/208642#M17764</guid>
      <dc:creator>roberto_m</dc:creator>
      <dc:date>2010-07-09T18:54:40Z</dc:date>
    </item>
    <item>
      <title>Re: My 12LED charlieplexing on a RS08KA</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/My-12LED-charlieplexing-on-a-RS08KA/m-p/208643#M17765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Groovy, man!&amp;nbsp; Nice work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jul 2010 21:51:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/My-12LED-charlieplexing-on-a-RS08KA/m-p/208643#M17765</guid>
      <dc:creator>irob</dc:creator>
      <dc:date>2010-07-09T21:51:57Z</dc:date>
    </item>
    <item>
      <title>Re: My 12LED charlieplexing on a RS08KA</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/My-12LED-charlieplexing-on-a-RS08KA/m-p/208644#M17766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Roberto,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For&amp;nbsp;this arrangement, and with only a single pin active (low) during stop mode,&amp;nbsp;and the other&amp;nbsp;three pins as KBI inputs, wakeup would be available for only three of the twelve switches.&amp;nbsp; If two pins were made actve during stop mode, the quantity would increase to four switches.&amp;nbsp; With three pins active, we are back to wakeup from&amp;nbsp;three switches.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However,&amp;nbsp;a comprehensive wakeup&amp;nbsp;might possibly be feasible if a fifth pin were available.&amp;nbsp; Four additional diodes would be required, with each anode connected to the existing diode anodes, and with the cathodes combined at the new pin.&amp;nbsp; This pin would remain active low during stop mode, and would be set to&amp;nbsp;logic&amp;nbsp;high&amp;nbsp;during the normal scanning process.&amp;nbsp; This will&amp;nbsp;require two pins fewer than a conventional 4 x 3 switch matrix.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If your Vdd supply is 3 volts, or less, I would recommend that all diodes be of the Schottky type&amp;nbsp;giving a lower forward voltage.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jul 2010 23:04:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/My-12LED-charlieplexing-on-a-RS08KA/m-p/208644#M17766</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-07-09T23:04:24Z</dc:date>
    </item>
  </channel>
</rss>