<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: OSC2 PIN AS GPIO OF MC908JL3ECDWE in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/OSC2-PIN-AS-GPIO-OF-MC908JL3ECDWE/m-p/208114#M17670</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;DIV&gt;The following alternatives might be a possibility. For example, the MC9S08AW16 is likely to be about the same price as the 908JL3E, and the MC9S08AC16 will likely be even cheaper.&amp;nbsp; These 44-pin devices should operate from the same voltage range as the current device.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Apr 2008 11:00:51 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2008-04-02T11:00:51Z</dc:date>
    <item>
      <title>OSC2 PIN AS GPIO OF MC908JL3ECDWE</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/OSC2-PIN-AS-GPIO-OF-MC908JL3ECDWE/m-p/208112#M17668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN style=": ; font-size: 2; font-family: Arial;"&gt;Hi&lt;BR /&gt;&lt;BR /&gt;I am using Freescale chip MC908JL3ECDWE.As per my application need,I am using External RC oscillator.&lt;BR /&gt;Now OSC2 pin is available free and can be configured as a general purpose I/O pin PTA6 or as KBI(Keyboard Interrupt)&lt;BR /&gt;&lt;BR /&gt;I have tried number of ways by doing manual coding, use of processor expert and beans on Code Warrior Compiler&lt;BR /&gt;in C language but couldn't get the result.&lt;BR /&gt;&lt;BR /&gt;As per application need, it' has to be configured as INPUT pin but&amp;nbsp; that&amp;nbsp; particular pin is having floating voltage,approx&lt;BR /&gt;2.5V in all attempts.&lt;BR /&gt;&lt;BR /&gt;Please help me out,I am very new to Freescale Micros.&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Apr 2008 00:35:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/OSC2-PIN-AS-GPIO-OF-MC908JL3ECDWE/m-p/208112#M17668</guid>
      <dc:creator>NaveenKumar</dc:creator>
      <dc:date>2008-04-01T00:35:29Z</dc:date>
    </item>
    <item>
      <title>Re: OSC2 PIN AS GPIO OF MC908JL3ECDWE</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/OSC2-PIN-AS-GPIO-OF-MC908JL3ECDWE/m-p/208113#M17669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello, and welcome to the forum.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;My understanding from the datasheet is that a different part number is required for the RC oscillator,&amp;nbsp;than that&amp;nbsp;with the crystal oscillator.&amp;nbsp; This is an old device, and the part numbering system has now changed.&amp;nbsp; Using the old part numbers, the standard part was MC68HC908JL3E, whereas the RC oscillator part was MC68H&lt;FONT color="#ff0000"&gt;R&lt;/FONT&gt;C908JL3E.&amp;nbsp; I am not sure whether the RC oscillator part is still available.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;An alternative would be to select a device from the 9S08 family.&amp;nbsp; These have an internal oscillator module, so don't consume any pins when this option is used.&amp;nbsp; Perhaps select a device that has 8K of flash, and that&amp;nbsp;is available in either 28-pin or 32-pin SM package.&amp;nbsp;&amp;nbsp;Maybe even&amp;nbsp;select a 44-pin package and you will have plenty of I/O available.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Apr 2008 10:25:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/OSC2-PIN-AS-GPIO-OF-MC908JL3ECDWE/m-p/208113#M17669</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-04-02T10:25:24Z</dc:date>
    </item>
    <item>
      <title>Re: OSC2 PIN AS GPIO OF MC908JL3ECDWE</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/OSC2-PIN-AS-GPIO-OF-MC908JL3ECDWE/m-p/208114#M17670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;DIV&gt;The following alternatives might be a possibility. For example, the MC9S08AW16 is likely to be about the same price as the 908JL3E, and the MC9S08AC16 will likely be even cheaper.&amp;nbsp; These 44-pin devices should operate from the same voltage range as the current device.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Apr 2008 11:00:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/OSC2-PIN-AS-GPIO-OF-MC908JL3ECDWE/m-p/208114#M17670</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-04-02T11:00:51Z</dc:date>
    </item>
    <item>
      <title>Re: OSC2 PIN AS GPIO OF MC908JL3ECDWE</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/OSC2-PIN-AS-GPIO-OF-MC908JL3ECDWE/m-p/208115#M17671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;bigmac wrote:&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;My understanding from the datasheet is that a different part number is required for the RC oscillator,&amp;nbsp;than that&amp;nbsp;with the crystal oscillator.&amp;nbsp; This is an old device, and the part numbering system has now changed.&amp;nbsp; Using the old part numbers, the standard part was MC68HC908JL3E, whereas the RC oscillator part was MC68H&lt;FONT color="#ff0000"&gt;R&lt;/FONT&gt;C908JL3E.&amp;nbsp; I am not sure whether the RC oscillator part is still available.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;BR /&gt;The above is certainly all true for the JK1 as I used the HRC and changed to the HC when they stopped the RC one. (with a crystal etc jammed in where the RC was) As they share the same datasheet I imagine this all hold true for the JL3.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Apr 2008 14:42:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/OSC2-PIN-AS-GPIO-OF-MC908JL3ECDWE/m-p/208115#M17671</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2008-04-02T14:42:45Z</dc:date>
    </item>
  </channel>
</rss>