<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: problem with QD2</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/problem-with-QD2/m-p/208093#M17667</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello, and welcome to the forum.&lt;BR /&gt;&lt;BR /&gt;Are you suggesting that Vbat is present whilst Vmicon is not present?&amp;nbsp; If so, you are likely to have in the region of 3 volts continuously applied to the PTA3 pin.&amp;nbsp; If Vmicon is not present, it is possible for an internal (intrinsic) diode to the Vdd rail to conduct, so that the Vdd voltage never reaches a sufficiently low voltage for POR to correctly occur.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Also keep in mind that the reference voltage for the ADC is supplied from Vdd.&amp;nbsp; This would mean that, if an ADC conversion should succeed under these conditions, the 8-bit result would remain at 255, resulting in PTA0 high.&lt;BR /&gt;&lt;BR /&gt;You will likely need additional circuitry to ensure that the voltage applied to PTA3 is clamped to zero in the absence of Vmicon.&lt;BR /&gt;&lt;BR /&gt;I also notice that the circuitry surrounding RED_LED seems a little peculiar - a LED current in the region of 0.1 mA, with a transistor base drive current of about 3 mA.&amp;nbsp; If the LED needs to conduct when PTA4 is low, you might consider using a PNP transistor.&amp;nbsp; For load currents of a few milliamps, the series resistor to the base should usually be somewhat higher than 1k.&lt;BR /&gt;&lt;BR /&gt;Not sure whether you require the additional pullup resistors, where external circuitry is driven by an output pin of the MCU.&lt;BR /&gt;&lt;BR /&gt;Within your code, consider using &lt;FONT face="Courier New"&gt;if-else&lt;/FONT&gt; constructs.&lt;BR /&gt;&lt;BR /&gt;&lt;FONT face="Courier New"&gt;#define PWM&amp;nbsp; PTAD_PTAD0&lt;BR /&gt;&lt;BR /&gt;if (bat_vol &amp;lt; 200)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; PWM = 0;&lt;BR /&gt;else&lt;BR /&gt;&amp;nbsp;&amp;nbsp; PWM = 1;&lt;/FONT&gt;&lt;BR /&gt;&lt;BR /&gt;This should be more efficient than using two separate &lt;FONT face="Courier New"&gt;if&lt;/FONT&gt; statements.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mac&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Dec 2008 10:07:32 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2008-12-09T10:07:32Z</dc:date>
    <item>
      <title>problem with QD2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/problem-with-QD2/m-p/208092#M17666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using QD2 for a battery management &amp;amp; High Power LED Driving application. Below are the details &amp;amp; problems along with the attached schematic.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;battery - 6V sealed lead acid,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;voltage regulator used - 3.3 V&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;battery disconnect - 5.7 V&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Battery reconnect - 6.0V&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;battery over voltage protection - 7.2V&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;please find the attached schematic. the microcontroller is behaving eratically during the discharge condition. The port pin PTA0 is going high if i switch on the supply for the micon during the hysterisis. can some body please help me resolve this issue. Also let me know if any hardware changes have to be done.i also have problems using BKGD &amp;amp; RESET pin.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Dec 2008 21:57:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/problem-with-QD2/m-p/208092#M17666</guid>
      <dc:creator>vinayprasad</dc:creator>
      <dc:date>2008-12-08T21:57:19Z</dc:date>
    </item>
    <item>
      <title>Re: problem with QD2</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/problem-with-QD2/m-p/208093#M17667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello, and welcome to the forum.&lt;BR /&gt;&lt;BR /&gt;Are you suggesting that Vbat is present whilst Vmicon is not present?&amp;nbsp; If so, you are likely to have in the region of 3 volts continuously applied to the PTA3 pin.&amp;nbsp; If Vmicon is not present, it is possible for an internal (intrinsic) diode to the Vdd rail to conduct, so that the Vdd voltage never reaches a sufficiently low voltage for POR to correctly occur.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Also keep in mind that the reference voltage for the ADC is supplied from Vdd.&amp;nbsp; This would mean that, if an ADC conversion should succeed under these conditions, the 8-bit result would remain at 255, resulting in PTA0 high.&lt;BR /&gt;&lt;BR /&gt;You will likely need additional circuitry to ensure that the voltage applied to PTA3 is clamped to zero in the absence of Vmicon.&lt;BR /&gt;&lt;BR /&gt;I also notice that the circuitry surrounding RED_LED seems a little peculiar - a LED current in the region of 0.1 mA, with a transistor base drive current of about 3 mA.&amp;nbsp; If the LED needs to conduct when PTA4 is low, you might consider using a PNP transistor.&amp;nbsp; For load currents of a few milliamps, the series resistor to the base should usually be somewhat higher than 1k.&lt;BR /&gt;&lt;BR /&gt;Not sure whether you require the additional pullup resistors, where external circuitry is driven by an output pin of the MCU.&lt;BR /&gt;&lt;BR /&gt;Within your code, consider using &lt;FONT face="Courier New"&gt;if-else&lt;/FONT&gt; constructs.&lt;BR /&gt;&lt;BR /&gt;&lt;FONT face="Courier New"&gt;#define PWM&amp;nbsp; PTAD_PTAD0&lt;BR /&gt;&lt;BR /&gt;if (bat_vol &amp;lt; 200)&lt;BR /&gt;&amp;nbsp;&amp;nbsp; PWM = 0;&lt;BR /&gt;else&lt;BR /&gt;&amp;nbsp;&amp;nbsp; PWM = 1;&lt;/FONT&gt;&lt;BR /&gt;&lt;BR /&gt;This should be more efficient than using two separate &lt;FONT face="Courier New"&gt;if&lt;/FONT&gt; statements.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mac&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Dec 2008 10:07:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/problem-with-QD2/m-p/208093#M17667</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-12-09T10:07:32Z</dc:date>
    </item>
  </channel>
</rss>