<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollersのトピックstack ram in 9s08JM60, JM32</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/stack-ram-in-9s08JM60-JM32/m-p/208020#M17661</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;A strange thing!&lt;/P&gt;&lt;P&gt;I have the stack pointer set to $1000, to use the top end of the 4K ram in the 9S08JM60.&lt;/P&gt;&lt;P&gt;The same code runs in the JM32 part, even though it is supposed to have only 2K ram (ending&amp;nbsp; at $0800) !&lt;/P&gt;&lt;P&gt;Maybe this part has the ram but is not production verified?&lt;/P&gt;&lt;P&gt;Any one know?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 20 Jun 2010 06:32:14 GMT</pubDate>
    <dc:creator>donw</dc:creator>
    <dc:date>2010-06-20T06:32:14Z</dc:date>
    <item>
      <title>stack ram in 9s08JM60, JM32</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/stack-ram-in-9s08JM60-JM32/m-p/208020#M17661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;A strange thing!&lt;/P&gt;&lt;P&gt;I have the stack pointer set to $1000, to use the top end of the 4K ram in the 9S08JM60.&lt;/P&gt;&lt;P&gt;The same code runs in the JM32 part, even though it is supposed to have only 2K ram (ending&amp;nbsp; at $0800) !&lt;/P&gt;&lt;P&gt;Maybe this part has the ram but is not production verified?&lt;/P&gt;&lt;P&gt;Any one know?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Jun 2010 06:32:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/stack-ram-in-9s08JM60-JM32/m-p/208020#M17661</guid>
      <dc:creator>donw</dc:creator>
      <dc:date>2010-06-20T06:32:14Z</dc:date>
    </item>
    <item>
      <title>Re: stack ram in 9s08JM60, JM32</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/stack-ram-in-9s08JM60-JM32/m-p/208021#M17662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is very common in the early months of production for smaller devices to actually have the die from a larger device.&lt;/P&gt;&lt;P&gt;This has been verified as being so on many different models.&lt;/P&gt;&lt;P&gt;Supposedly Freescale only test the quoted amount of memory.&lt;/P&gt;&lt;P&gt;Generally it stops being like this at some indeterminate point.&lt;/P&gt;&lt;P&gt;So enjoy it while you can!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Jun 2010 06:39:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/stack-ram-in-9s08JM60-JM32/m-p/208021#M17662</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2010-06-20T06:39:45Z</dc:date>
    </item>
  </channel>
</rss>