<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: Shelf Life Of device</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Shelf-Life-Of-device-MC68HC908JK8/m-p/207839#M17641</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The "shelf life" is likely to depend on whether the device is already mounted to the circuit board, or not, and the conditions under which the storage takes place.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If the storage takes place prior to being mounted, maintaining solderability of the pins is likely to be the main issue.&amp;nbsp; Storage in a damp "tropical" climate is likely to be a problem, especially if fungal growth can occur.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;It is possible for the device&amp;nbsp;package to absorb moisture over time.&amp;nbsp; With SM devices, this can give reliability problems during the reflow soldering process, unless baked for a lengthy period prior to use.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;These considerations would dictate that, for&amp;nbsp;long term storage,&amp;nbsp;sealed packing should be used, that incorporates a desiccant.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 29 Mar 2008 22:02:35 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2008-03-29T22:02:35Z</dc:date>
    <item>
      <title>Shelf Life Of device - MC68HC908JK8</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Shelf-Life-Of-device-MC68HC908JK8/m-p/207837#M17639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Dear Sir,&lt;/DIV&gt;&lt;DIV&gt;I am using MC68HC908JK8.I would like to know What is the Shelf Life of the device MC68HC908JK8 OR any 8 bit device.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Added part number to subject&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by NLFSJ on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2008-03-29&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;10:47 AM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Mar 2008 18:17:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Shelf-Life-Of-device-MC68HC908JK8/m-p/207837#M17639</guid>
      <dc:creator>Deepak1</dc:creator>
      <dc:date>2008-03-29T18:17:25Z</dc:date>
    </item>
    <item>
      <title>Re: Shelf Life Of device</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Shelf-Life-Of-device-MC68HC908JK8/m-p/207838#M17640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;1000 Years at room temperature.&lt;BR /&gt;Now that I have said that, lets be more conservative and say 100 years.&lt;BR /&gt;At room temperature the Flash is specified&amp;nbsp; by Freescale to remember it's data for 100 years, so I would guess that would mean the part is good for a least 100 years.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Mar 2008 21:09:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Shelf-Life-Of-device-MC68HC908JK8/m-p/207838#M17640</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-03-29T21:09:33Z</dc:date>
    </item>
    <item>
      <title>Re: Shelf Life Of device</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Shelf-Life-Of-device-MC68HC908JK8/m-p/207839#M17641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The "shelf life" is likely to depend on whether the device is already mounted to the circuit board, or not, and the conditions under which the storage takes place.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If the storage takes place prior to being mounted, maintaining solderability of the pins is likely to be the main issue.&amp;nbsp; Storage in a damp "tropical" climate is likely to be a problem, especially if fungal growth can occur.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;It is possible for the device&amp;nbsp;package to absorb moisture over time.&amp;nbsp; With SM devices, this can give reliability problems during the reflow soldering process, unless baked for a lengthy period prior to use.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;These considerations would dictate that, for&amp;nbsp;long term storage,&amp;nbsp;sealed packing should be used, that incorporates a desiccant.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Mac&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Mar 2008 22:02:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Shelf-Life-Of-device-MC68HC908JK8/m-p/207839#M17641</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2008-03-29T22:02:35Z</dc:date>
    </item>
    <item>
      <title>Re: Shelf Life Of device</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Shelf-Life-Of-device-MC68HC908JK8/m-p/207840#M17642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Agreed, but I would take shelf life to mean stored as per some specification.&lt;BR /&gt;If the part is mounted in a board, you have an entirely different set of parameters.&lt;BR /&gt;&lt;BR /&gt;The expiration on a carton of milk assumes a set of storage conditions, not after you pour it in a glass (i.e. remove it from its "factory" container). And that of course it is at a certain temperature.&lt;BR /&gt;&lt;BR /&gt;Note to that ROHS could add a whole new dimension to this.&lt;BR /&gt;&lt;BR /&gt;You should &lt;A href="http://www.edn.com/article/CA6477864.html" rel="nofollow" target="_blank"&gt;read this.&lt;/A&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Mar 2008 22:51:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Shelf-Life-Of-device-MC68HC908JK8/m-p/207840#M17642</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-03-29T22:51:40Z</dc:date>
    </item>
    <item>
      <title>Re: Shelf Life Of device</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Shelf-Life-Of-device-MC68HC908JK8/m-p/207841#M17643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thank for reply,&lt;/DIV&gt;&lt;DIV&gt;Without Opening factory Package how long we can keep the device as it is &amp;amp; what precaution should we take before usage.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Mar 2008 12:48:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Shelf-Life-Of-device-MC68HC908JK8/m-p/207841#M17643</guid>
      <dc:creator>Deepak1</dc:creator>
      <dc:date>2008-03-30T12:48:54Z</dc:date>
    </item>
  </channel>
</rss>