<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Visualization Tools - True Time Simulator in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Visualization-Tools-True-Time-Simulator/m-p/207232#M17549</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Attached a small project, with a visualization tool component allowing you to toggle PTA2.&lt;/DIV&gt;&lt;DIV&gt;Just rebuild the project.&lt;/DIV&gt;&lt;DIV&gt;Once in the debugger, when you are stopped at main do a Step Over to make sure the function PE_low_level_init is executed and all peripherals are initialized properly.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;After that you can click on the LED or Switch instrument to toggle PTA2.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Dec 2008 22:26:43 GMT</pubDate>
    <dc:creator>CrasyCat</dc:creator>
    <dc:date>2008-12-05T22:26:43Z</dc:date>
    <item>
      <title>Visualization Tools - True Time Simulator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Visualization-Tools-True-Time-Simulator/m-p/207229#M17546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Is it possible, with Visualization Tools&amp;nbsp; (embedded True Time Simulator SW), to put an instrument like button connected as input and not output ?&lt;/DIV&gt;&lt;DIV&gt;For exemple i would like connect a push button on PTAD2 to simulate a KBI isr because i have not yet HW board.&lt;/DIV&gt;&lt;DIV&gt;For instance, with Visualization Tools, i can just display the output state of PORT.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks for your help&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;David&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Dec 2008 23:32:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Visualization-Tools-True-Time-Simulator/m-p/207229#M17546</guid>
      <dc:creator>DavidoBG</dc:creator>
      <dc:date>2008-12-04T23:32:26Z</dc:date>
    </item>
    <item>
      <title>Re: Visualization Tools - True Time Simulator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Visualization-Tools-True-Time-Simulator/m-p/207230#M17547</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You can stimulate input to a bit within an I/O port using the visualization tool, but I&amp;nbsp;am not sure you can &amp;nbsp;raise an interrupt from this window.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;To connect an instrument to PTD2:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; - Add either a LED or Switch Instrument to your visualization window&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; - Click with the right mouse button on the instrument and select Properties&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; - Set Port to Display to 0x6&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; - Set Bit Number to display to 2&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; - Close the Property dialog&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp; - Switch the visualization window from Edit Mode to Display Mode&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (Click with&amp;nbsp;the right button in&amp;nbsp;the window and make sure "Edit Mode" is unchecked in&amp;nbsp;the menu).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;While application is running it should be possible to toggle the bit 2 in PORTD&amp;nbsp;clicking on the instrument.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am not sure the KBI interrupt will raise, but it might be worth a try.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Dec 2008 18:56:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Visualization-Tools-True-Time-Simulator/m-p/207230#M17547</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2008-12-05T18:56:31Z</dc:date>
    </item>
    <item>
      <title>Re: Visualization Tools - True Time Simulator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Visualization-Tools-True-Time-Simulator/m-p/207231#M17548</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I follow your instructions crasycat but i cannot toggle button. I seems, the button display the output state of this port.&lt;/DIV&gt;&lt;DIV&gt;Do you have any vtl sample file. I use MS9S08QE8&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks David&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Dec 2008 21:34:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Visualization-Tools-True-Time-Simulator/m-p/207231#M17548</guid>
      <dc:creator>DavidoBG</dc:creator>
      <dc:date>2008-12-05T21:34:26Z</dc:date>
    </item>
    <item>
      <title>Re: Visualization Tools - True Time Simulator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Visualization-Tools-True-Time-Simulator/m-p/207232#M17549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Attached a small project, with a visualization tool component allowing you to toggle PTA2.&lt;/DIV&gt;&lt;DIV&gt;Just rebuild the project.&lt;/DIV&gt;&lt;DIV&gt;Once in the debugger, when you are stopped at main do a Step Over to make sure the function PE_low_level_init is executed and all peripherals are initialized properly.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;After that you can click on the LED or Switch instrument to toggle PTA2.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;CrasyCat&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Dec 2008 22:26:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Visualization-Tools-True-Time-Simulator/m-p/207232#M17549</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2008-12-05T22:26:43Z</dc:date>
    </item>
    <item>
      <title>Re: Visualization Tools - True Time Simulator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Visualization-Tools-True-Time-Simulator/m-p/207233#M17550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;OK that's right, thanks&lt;/DIV&gt;&lt;DIV&gt;David&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Dec 2008 22:54:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Visualization-Tools-True-Time-Simulator/m-p/207233#M17550</guid>
      <dc:creator>DavidoBG</dc:creator>
      <dc:date>2008-12-05T22:54:26Z</dc:date>
    </item>
  </channel>
</rss>