<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: QG8 internal pullup = 150uA???</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-internal-pullup-150uA/m-p/207118#M17513</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;You wouldn't happen to have the KBEDG1 bit set, do you? If set this would make the internal resistor a pulldown rather than a pullup. Not having seen your circuit I don't know if this is relevant or not.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 06 Dec 2008 04:14:22 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2008-12-06T04:14:22Z</dc:date>
    <item>
      <title>QG8 internal pullup = 150uA???</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-internal-pullup-150uA/m-p/207114#M17509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Hi Folks,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I must be missing something - I'm working on reducing current consumption on a&lt;/DIV&gt;&lt;DIV&gt;battery device, and it's drawing about 150 uA more than it should in STOP3 mode.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I narrowed it down to when I select an internal pullup with PTAPE.&amp;nbsp; If no pullup is&lt;/DIV&gt;&lt;DIV&gt;selected, the current is basically nothing.&amp;nbsp; With it, it is 150uA.&amp;nbsp; It is PTA1, and I'm&lt;/DIV&gt;&lt;DIV&gt;using it as a keyboard interrupt.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If I&amp;nbsp;put an external pullup on it (for a switch),&amp;nbsp;the circuit works fine, and there&lt;/DIV&gt;&lt;DIV&gt;is no extra current.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Ideas?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks,&lt;/DIV&gt;&lt;DIV&gt;&lt;BR /&gt;Tim&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Dec 2008 09:35:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-internal-pullup-150uA/m-p/207114#M17509</guid>
      <dc:creator>UtopiaTim</dc:creator>
      <dc:date>2008-12-04T09:35:53Z</dc:date>
    </item>
    <item>
      <title>Re: QG8 internal pullup = 150uA???</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-internal-pullup-150uA/m-p/207115#M17510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;150uA seems resonable to me. 3.3V / 150u = 22kOhm.&lt;BR /&gt;&lt;BR /&gt;I might have misunderstood the problem, but how exactly do you expect a pull-up to work with 0A current through it?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Dec 2008 17:52:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-internal-pullup-150uA/m-p/207115#M17510</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2008-12-04T17:52:48Z</dc:date>
    </item>
    <item>
      <title>Re: QG8 internal pullup = 150uA???</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-internal-pullup-150uA/m-p/207116#M17511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Ah, I presume he meant with the switch open.&lt;BR /&gt;With it closed you should see something like this (probably a fair bit less)&lt;BR /&gt;A pullup will work with virtually no current when it is pulling up a CMOS input gate.&lt;BR /&gt;A Utopian one&lt;SPAN&gt;&lt;IMG alt=":smileyvery-happy:" class="emoticon emoticon-smileyvery-happy" id="smileyvery-happy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-very-happy.gif" title="Smiley Very Happy" /&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Dec 2008 20:39:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-internal-pullup-150uA/m-p/207116#M17511</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2008-12-04T20:39:14Z</dc:date>
    </item>
    <item>
      <title>Re: QG8 internal pullup = 150uA???</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-internal-pullup-150uA/m-p/207117#M17512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;Cute! &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Yes, it's with the switch open.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I'm not worried about the current when the switch is closed (it's minimal&lt;/DIV&gt;&lt;DIV&gt;compared to what the rest of the circuit is drawing).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Guess I'll put a pullup on the board, &amp;amp; if I figure it out before production,&lt;/DIV&gt;&lt;DIV&gt;it'll just be a no populate.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Tim&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Dec 2008 22:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-internal-pullup-150uA/m-p/207117#M17512</guid>
      <dc:creator>UtopiaTim</dc:creator>
      <dc:date>2008-12-04T22:38:55Z</dc:date>
    </item>
    <item>
      <title>Re: QG8 internal pullup = 150uA???</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-internal-pullup-150uA/m-p/207118#M17513</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;You wouldn't happen to have the KBEDG1 bit set, do you? If set this would make the internal resistor a pulldown rather than a pullup. Not having seen your circuit I don't know if this is relevant or not.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Dec 2008 04:14:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-internal-pullup-150uA/m-p/207118#M17513</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2008-12-06T04:14:22Z</dc:date>
    </item>
    <item>
      <title>Re: QG8 internal pullup = 150uA???</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-internal-pullup-150uA/m-p/207119#M17514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Wingsy,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Checked, and the bit is clear - set for falling edge.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Tim&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Dec 2008 05:02:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/QG8-internal-pullup-150uA/m-p/207119#M17514</guid>
      <dc:creator>UtopiaTim</dc:creator>
      <dc:date>2008-12-06T05:02:40Z</dc:date>
    </item>
  </channel>
</rss>