<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: Interrupt Routine for MC9S08LC60.</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Interrupt-Routine-for-MC9S08LC60/m-p/207102#M17504</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello FWFan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The FAQ section of AN2616 briefly describes a number of methods for coding ISRs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, perhaps you are using an early version of the header file.&amp;nbsp; The 'LC60 header file&amp;nbsp;contained within CW 6.3 certainly&amp;nbsp;defines macros for the vector numbers.&amp;nbsp; Of course, you can simply use the vector number in lieu of the macro.&amp;nbsp; The vector number is easily determined, by counting backwards the number of words from the reset vector (0xFFFE), to the vector address of interest.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Jun 2010 10:58:35 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2010-06-16T10:58:35Z</dc:date>
    <item>
      <title>Interrupt Routine for MC9S08LC60.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Interrupt-Routine-for-MC9S08LC60/m-p/207101#M17503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do you write an interrupt for the MC9S08LC60?&lt;/P&gt;&lt;P&gt;Usually there's the Vectornumber_*_* for the MC9S08QE128,&lt;/P&gt;&lt;P&gt;but the LC60 doesn't have the vector number table in the&lt;/P&gt;&lt;P&gt;device .h file.&amp;nbsp; Could you show me how?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;FWFan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jun 2010 01:29:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Interrupt-Routine-for-MC9S08LC60/m-p/207101#M17503</guid>
      <dc:creator>FWFan</dc:creator>
      <dc:date>2010-06-16T01:29:08Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt Routine for MC9S08LC60.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Interrupt-Routine-for-MC9S08LC60/m-p/207102#M17504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello FWFan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The FAQ section of AN2616 briefly describes a number of methods for coding ISRs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, perhaps you are using an early version of the header file.&amp;nbsp; The 'LC60 header file&amp;nbsp;contained within CW 6.3 certainly&amp;nbsp;defines macros for the vector numbers.&amp;nbsp; Of course, you can simply use the vector number in lieu of the macro.&amp;nbsp; The vector number is easily determined, by counting backwards the number of words from the reset vector (0xFFFE), to the vector address of interest.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jun 2010 10:58:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Interrupt-Routine-for-MC9S08LC60/m-p/207102#M17504</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-06-16T10:58:35Z</dc:date>
    </item>
    <item>
      <title>Re: Interrupt Routine for MC9S08LC60.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Interrupt-Routine-for-MC9S08LC60/m-p/207103#M17505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you bigmac.&amp;nbsp; That was a big help.&amp;nbsp; I got it to work following that app. note.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Much appreciated.&lt;/P&gt;&lt;P&gt;FWFan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jun 2010 02:03:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Interrupt-Routine-for-MC9S08LC60/m-p/207103#M17505</guid>
      <dc:creator>FWFan</dc:creator>
      <dc:date>2010-06-17T02:03:41Z</dc:date>
    </item>
  </channel>
</rss>