<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Contiguous Flash in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Contiguous-Flash/m-p/206956#M17480</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The MC9S08LC36 MCU has two Flash memories that are not contiguous.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do I have to worry if my program is placed in between the memories as if it were a contiguous memory space?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Jun 2010 17:55:41 GMT</pubDate>
    <dc:creator>rdazcal</dc:creator>
    <dc:date>2010-06-15T17:55:41Z</dc:date>
    <item>
      <title>Contiguous Flash</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Contiguous-Flash/m-p/206956#M17480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The MC9S08LC36 MCU has two Flash memories that are not contiguous.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do I have to worry if my program is placed in between the memories as if it were a contiguous memory space?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jun 2010 17:55:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Contiguous-Flash/m-p/206956#M17480</guid>
      <dc:creator>rdazcal</dc:creator>
      <dc:date>2010-06-15T17:55:41Z</dc:date>
    </item>
    <item>
      <title>Re: Contiguous Flash</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Contiguous-Flash/m-p/206957#M17481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The contents of the PRM file for the project enable the linker to determine which address ranges are read-only, for the purpose of placing code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The one exception is an absolute assembly project, where the linker is not used.&amp;nbsp; Here it is the responsibility of the programmer to determine&amp;nbsp;a suitable&amp;nbsp;code placement.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jun 2010 11:23:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Contiguous-Flash/m-p/206957#M17481</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2010-06-16T11:23:40Z</dc:date>
    </item>
  </channel>
</rss>