<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC1322x USB dongle in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1322x-USB-dongle/m-p/206819#M17447</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It works with WireShark to capture packets.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Install &lt;A href="http://wireshark.org/" rel="nofollow" target="_self"&gt;WireShark&lt;/A&gt; and the &lt;A href="http://sourceforge.net/projects/wiresharkzigbee/" rel="nofollow" target="_self"&gt;WireShark ZigBee&lt;/A&gt; Utility.&amp;nbsp; You launch the utility from a command-prompt, passing in the COM port of the USB Dongle and the ZigBee channel you want to sniff.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then you go into Wireshark and paste "\\.\pipe\wireshark" into the Interface field of teh Capture Options dialog.&amp;nbsp; Wireshark will then start displaying and decoding captured packets.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Apr 2011 06:07:03 GMT</pubDate>
    <dc:creator>tomlogic</dc:creator>
    <dc:date>2011-04-22T06:07:03Z</dc:date>
    <item>
      <title>MC1322x USB dongle</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1322x-USB-dongle/m-p/206818#M17446</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm looking for some description of the MC1322x USB dongle pre installed sniffer firmware (or for the source code of it).&lt;/P&gt;&lt;P&gt;I'd like to communicate with the device through virtual COM and I need to know what are the commands available.&lt;/P&gt;&lt;P&gt;Does anybody know where to find such a documentation?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2009 01:13:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1322x-USB-dongle/m-p/206818#M17446</guid>
      <dc:creator>Nyarlathotep</dc:creator>
      <dc:date>2009-08-13T01:13:29Z</dc:date>
    </item>
    <item>
      <title>Re: MC1322x USB dongle</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1322x-USB-dongle/m-p/206819#M17447</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It works with WireShark to capture packets.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Install &lt;A href="http://wireshark.org/" rel="nofollow" target="_self"&gt;WireShark&lt;/A&gt; and the &lt;A href="http://sourceforge.net/projects/wiresharkzigbee/" rel="nofollow" target="_self"&gt;WireShark ZigBee&lt;/A&gt; Utility.&amp;nbsp; You launch the utility from a command-prompt, passing in the COM port of the USB Dongle and the ZigBee channel you want to sniff.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then you go into Wireshark and paste "\\.\pipe\wireshark" into the Interface field of teh Capture Options dialog.&amp;nbsp; Wireshark will then start displaying and decoding captured packets.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Apr 2011 06:07:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC1322x-USB-dongle/m-p/206819#M17447</guid>
      <dc:creator>tomlogic</dc:creator>
      <dc:date>2011-04-22T06:07:03Z</dc:date>
    </item>
  </channel>
</rss>