<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: BDM problem on MC9S08LL16</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BDM-problem-on-MC9S08LL16/m-p/206535#M17408</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are many things that could cause such problems. The far most common ones are:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- The MCU could be secured. This is a feature of new MCUs that prevents copycats from stealing code. You can unsecure your MCU through a free program available from PE Micro's web site, or through the Codewarrior debugger.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Incorrect BDM or reset lines. Missing pull-ups on these lines. Missing ground between BDM connector and PC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- 2x3 socket header turned upside down 180 degrees, or the cables/connectors are damaged.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- CPU clock is missing because of wrong design or poorly soldered crystal. Make a rough measurement of the oscillator frequency with an oscilloscope to see that the MCU is alive and running at the desired speed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Poor power supply or no supply at all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Jun 2010 18:59:12 GMT</pubDate>
    <dc:creator>Lundin</dc:creator>
    <dc:date>2010-06-11T18:59:12Z</dc:date>
    <item>
      <title>BDM problem on MC9S08LL16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BDM-problem-on-MC9S08LL16/m-p/206534#M17407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am doing a project with MC9S08LL16. However, I can't download any program via a PE USB multilink interface. The codewarrior remind me a power cycle dialog saying that The target MCU is not reponding, turn MCU power on, and then click OK. It fails again&amp;nbsp;after I do as the same as the dialog upon. Now the coderwarrior gives me&amp;nbsp;another note "Failure connecting to device.Power cycle the HCS08 processor and try connecting again". I have check the power and ground of MCU, including BDM connection. But it seems that there is no mistakes. Thank you for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jun 2010 16:58:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/BDM-problem-on-MC9S08LL16/m-p/206534#M17407</guid>
      <dc:creator>VincentLau</dc:creator>
      <dc:date>2010-06-11T16:58:12Z</dc:date>
    </item>
    <item>
      <title>Re: BDM problem on MC9S08LL16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BDM-problem-on-MC9S08LL16/m-p/206535#M17408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are many things that could cause such problems. The far most common ones are:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- The MCU could be secured. This is a feature of new MCUs that prevents copycats from stealing code. You can unsecure your MCU through a free program available from PE Micro's web site, or through the Codewarrior debugger.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Incorrect BDM or reset lines. Missing pull-ups on these lines. Missing ground between BDM connector and PC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- 2x3 socket header turned upside down 180 degrees, or the cables/connectors are damaged.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- CPU clock is missing because of wrong design or poorly soldered crystal. Make a rough measurement of the oscillator frequency with an oscilloscope to see that the MCU is alive and running at the desired speed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Poor power supply or no supply at all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jun 2010 18:59:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/BDM-problem-on-MC9S08LL16/m-p/206535#M17408</guid>
      <dc:creator>Lundin</dc:creator>
      <dc:date>2010-06-11T18:59:12Z</dc:date>
    </item>
    <item>
      <title>Re: BDM problem on MC9S08LL16</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/BDM-problem-on-MC9S08LL16/m-p/206536#M17409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can I program with out the PE? Manual load?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Aug 2010 01:52:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/BDM-problem-on-MC9S08LL16/m-p/206536#M17409</guid>
      <dc:creator>jbond</dc:creator>
      <dc:date>2010-08-17T01:52:49Z</dc:date>
    </item>
  </channel>
</rss>