<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Trouble programming JM32 with DEMOQE</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Trouble-programming-JM32-with-DEMOQE/m-p/206360#M17388</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I'm having a heck of a time trying to debug/program a JM32 using a DEMOQE board's built in BDM multilink interface.&amp;nbsp; I just have the bare essentials as far as the JM32 setup...basically what they have in the Data sheet near the beginning setup for 5V.&amp;nbsp; Without the BDM, both reset and bkgd are pulled to 5V.&amp;nbsp; With the BDM pod connected, reset immediately drops to 3.82 V, the highest the BKGD pin goes is 2.54V when trying to connect inside the True-time Simulator/debugger.&amp;nbsp; I get an error in the True time console: Error: Can not enter background mode&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I noticed on the DEMOQE schematic there is a 4.7k pullup installed as R3 on the BKGD line to its VDD, which is around 3.1V.&amp;nbsp; There is a 4.7k pullup on the schematic as R4 on the RESET line to VDD, but this resistor is not installed on my board.&amp;nbsp; I only installed 5 out of the 6 pins for the BDM connector on the DEMO board, I left out pin 6, VDD as I was wary of frying the DEMO board with my 5V target.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please correct me if I'm wrong but I thought the DEMOQE board could work with 5V targets.&amp;nbsp; Does anyone have experience doing this, and/or tell me what i'm doing wrong.&amp;nbsp; I have used the DEMOQE to debug a QG16 externally before, that worked fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Aaron&lt;/SPAN&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Dec 2008 07:32:59 GMT</pubDate>
    <dc:creator>protoease</dc:creator>
    <dc:date>2008-12-01T07:32:59Z</dc:date>
    <item>
      <title>Trouble programming JM32 with DEMOQE</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Trouble-programming-JM32-with-DEMOQE/m-p/206360#M17388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I'm having a heck of a time trying to debug/program a JM32 using a DEMOQE board's built in BDM multilink interface.&amp;nbsp; I just have the bare essentials as far as the JM32 setup...basically what they have in the Data sheet near the beginning setup for 5V.&amp;nbsp; Without the BDM, both reset and bkgd are pulled to 5V.&amp;nbsp; With the BDM pod connected, reset immediately drops to 3.82 V, the highest the BKGD pin goes is 2.54V when trying to connect inside the True-time Simulator/debugger.&amp;nbsp; I get an error in the True time console: Error: Can not enter background mode&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I noticed on the DEMOQE schematic there is a 4.7k pullup installed as R3 on the BKGD line to its VDD, which is around 3.1V.&amp;nbsp; There is a 4.7k pullup on the schematic as R4 on the RESET line to VDD, but this resistor is not installed on my board.&amp;nbsp; I only installed 5 out of the 6 pins for the BDM connector on the DEMO board, I left out pin 6, VDD as I was wary of frying the DEMO board with my 5V target.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please correct me if I'm wrong but I thought the DEMOQE board could work with 5V targets.&amp;nbsp; Does anyone have experience doing this, and/or tell me what i'm doing wrong.&amp;nbsp; I have used the DEMOQE to debug a QG16 externally before, that worked fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Aaron&lt;/SPAN&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Dec 2008 07:32:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Trouble-programming-JM32-with-DEMOQE/m-p/206360#M17388</guid>
      <dc:creator>protoease</dc:creator>
      <dc:date>2008-12-01T07:32:59Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble programming JM32 with DEMOQE</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Trouble-programming-JM32-with-DEMOQE/m-p/206361#M17389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;Get a DEMOJM board instead.&lt;/DIV&gt;&lt;DIV&gt;The DEMO boards have been designed to&amp;nbsp;support only the MCU that is in the extension.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Ake&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Dec 2008 18:02:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Trouble-programming-JM32-with-DEMOQE/m-p/206361#M17389</guid>
      <dc:creator>Ake</dc:creator>
      <dc:date>2008-12-01T18:02:46Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble programming JM32 with DEMOQE</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Trouble-programming-JM32-with-DEMOQE/m-p/206362#M17390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The DEMOJM board is $99, I would just buy the PE Multilink for that much.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I borrowed a Multilink from work and it works just fine, so it must be some level translation issue...&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Dec 2008 14:49:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Trouble-programming-JM32-with-DEMOQE/m-p/206362#M17390</guid>
      <dc:creator>protoease</dc:creator>
      <dc:date>2008-12-02T14:49:11Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble programming JM32 with DEMOQE</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Trouble-programming-JM32-with-DEMOQE/m-p/206363#M17391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I had the same problem when I got my blank 9S08QE32s.&amp;nbsp; I could not get the DEMOQE board (with a 6-pin header soldered in and cable to target) to program them, even though it will program the 9S08QE32 on the plug-in daughterboard just fine.&amp;nbsp; I even wire-wrapped to the pins on the DEMO board, straight to an SO-to-DIP adapter with the QE32 on it -- no joy.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I had to buy the USB-Multilink.&amp;nbsp; Had to cycle power on my target the first time, then it programmed fine.&amp;nbsp; In my application, I set the RESET and BKGD pins to perform those functions (instead of the defaults), and now it goes into debug just fine without cycling power.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I never got a good answer from P&amp;amp;E or Freescale as to why the DEMOQE (or DEMOQG8) on-board BDM won't program a blank QE32.&amp;nbsp; But it won't.&amp;nbsp; (I was able to use the DEMOQG8 on-board BDM to program blank QG8s.... go figure.)&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The chips on the daughterboards come pre-flashed with the demo application, which sets up RESET and BKGD, so the on-board BDM will work with them.&amp;nbsp; I bet if you unsoldered the chip from the daughterboard and soldered on a blank part, it wouldn't go into debug.....&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Probably intentional to keep from giving away free BDMs in the design contests....&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Dale, W8ABZ&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Dec 2008 11:47:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Trouble-programming-JM32-with-DEMOQE/m-p/206363#M17391</guid>
      <dc:creator>w8abz</dc:creator>
      <dc:date>2008-12-17T11:47:19Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble programming JM32 with DEMOQE</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Trouble-programming-JM32-with-DEMOQE/m-p/206364#M17392</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I am having a similar issue with trying to use my demo boards as a BDM interface.&amp;nbsp; Everything is fine in version 6.1&amp;nbsp; with 6.2 I need to use the JM demo board, as it won't let me use the AW demo board.&amp;nbsp; This is ok,&amp;nbsp; I have both demo boards (the QE demo as well)&amp;nbsp; But 6.2 will not connect to my JM target system, but it will connect to a JM chip if I install the daughter board.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Is there a reset connection thru the ribbon cable that is necessary (has not been in the past...)&amp;nbsp; Or other supporting connections?&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Bob&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Dec 2008 16:27:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Trouble-programming-JM32-with-DEMOQE/m-p/206364#M17392</guid>
      <dc:creator>TurboBob</dc:creator>
      <dc:date>2008-12-24T16:27:28Z</dc:date>
    </item>
  </channel>
</rss>