<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 DEMO9RS08KA2 Windows 7 64bit</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO9RS08KA2-Windows-7-64bit/m-p/206283#M17381</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I got a DEMO9RS08KA2 board, my computer is running Windows 7 64bit. I can't install the driver or CW 6.2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The USB to BDM Interface is using a MC9JB16FAE microcontroller.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My questions:&lt;/P&gt;&lt;P&gt;* Is there a way to get this demo board working with my current setup?&lt;/P&gt;&lt;P&gt;* Could it work with CW10.1?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Feb 2012 14:55:36 GMT</pubDate>
    <dc:creator>esaias_pech</dc:creator>
    <dc:date>2012-02-15T14:55:36Z</dc:date>
    <item>
      <title>DEMO9RS08KA2 Windows 7 64bit</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO9RS08KA2-Windows-7-64bit/m-p/206283#M17381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I got a DEMO9RS08KA2 board, my computer is running Windows 7 64bit. I can't install the driver or CW 6.2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The USB to BDM Interface is using a MC9JB16FAE microcontroller.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My questions:&lt;/P&gt;&lt;P&gt;* Is there a way to get this demo board working with my current setup?&lt;/P&gt;&lt;P&gt;* Could it work with CW10.1?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2012 14:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO9RS08KA2-Windows-7-64bit/m-p/206283#M17381</guid>
      <dc:creator>esaias_pech</dc:creator>
      <dc:date>2012-02-15T14:55:36Z</dc:date>
    </item>
    <item>
      <title>Re: DEMO9RS08KA2 Windows 7 64bit</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO9RS08KA2-Windows-7-64bit/m-p/206284#M17382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CW 6.x won't run in a WIN7 64 bit mode. There are many posts about this issue. Some have it working by replacing the driver DLL with newer compatible ones, but I could not get it working that way.&lt;/P&gt;&lt;P&gt;I (and others) use VMWARE (freeware) to create a virtual WinXP enviroment, and run CW 6.x in that.&lt;/P&gt;&lt;P&gt;Its very stable, Bit of a bother having to start the virtual machine, &amp;nbsp;but it runs OK.&lt;/P&gt;&lt;P&gt;Note that do this you will need a WIN XP install disk.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note also that CW 10.1 (or .3) under WIN7 64bit has some driver bug and won't connect to a DEMOJM60 board.&lt;/P&gt;&lt;P&gt;Last time I checked into this problem last year, P&amp;amp;E didn't have a WIN7 64bit machine to check out the problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2012 15:21:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/DEMO9RS08KA2-Windows-7-64bit/m-p/206284#M17382</guid>
      <dc:creator>donw</dc:creator>
      <dc:date>2012-02-15T15:21:22Z</dc:date>
    </item>
  </channel>
</rss>