<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Setting up a Free tool chain for HC908 on Mac OS X: SDCC,Eclipse,make and a Free bootloader</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Setting-up-a-Free-tool-chain-for-HC908-on-Mac-OS-X-SDCC-Eclipse/m-p/204951#M17069</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bob,&lt;/P&gt;&lt;P&gt;I just tried sdcc 3.1 with a S08js16.&lt;/P&gt;&lt;P&gt;For the JS16 the compile line should contain -mhc08 --data-loc 0x80 --code-loc 0xC400 --stack-loc 0x027F&lt;/P&gt;&lt;P&gt;interesting enough the stack-loc must be in the compile stage (not the linker as it does nothing there).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For flashing, it is likely you can port usbdm without much effort (based on wxwidgets and libusb which are both available on mac).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Feb 2012 12:21:08 GMT</pubDate>
    <dc:creator>ggorlik</dc:creator>
    <dc:date>2012-02-13T12:21:08Z</dc:date>
    <item>
      <title>Setting up a Free tool chain for HC908 on Mac OS X: SDCC,Eclipse,make and a Free bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Setting-up-a-Free-tool-chain-for-HC908-on-Mac-OS-X-SDCC-Eclipse/m-p/204949#M17067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;sorry to 'advertise' here but I've written a page or two to help beginners in microcontrollers (MC68HC908JB8) to get started.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It is about consrtructing a minimal hardware setup and setting a Free tool chain at under 15 USD in a couple of hours.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(I'm not selling anything, the price is the price of the parts from wherever you want to get them)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The tool chain uses SDCC, Eclipse, make and my free bootloader, bl08, and I've set it up on Mac OS X 10.4.11 but&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;should be trivial to set up in Linux, and should not be too bad on Windows if one uses Cygwin or MinGW to compile&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the bootloader.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To read the story, goto my website at:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.sparetimelabs.com%2F" rel="nofollow" target="_blank"&gt;http://www.sparetimelabs.com/&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;and select 'Fun with HC08' from the navigation on the left.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;To read about the bootloader select 'bl08'.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There is also something that might be of interest to SDCC user and embedded programmers on page 'PrintfII'.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;br Kusti&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Mar 2008 12:57:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Setting-up-a-Free-tool-chain-for-HC908-on-Mac-OS-X-SDCC-Eclipse/m-p/204949#M17067</guid>
      <dc:creator>kusti</dc:creator>
      <dc:date>2008-03-21T12:57:40Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up a Free tool chain for HC908 on Mac OS X: SDCC,Eclipse,make and a Free bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Setting-up-a-Free-tool-chain-for-HC908-on-Mac-OS-X-SDCC-Eclipse/m-p/204950#M17068</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kusti,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is great news. I am a FAE with Avnet and have three Freescale customers that would prefer﻿ to develop on the Mac. Have you done any development on this since 2008?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Sep 2011 00:07:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Setting-up-a-Free-tool-chain-for-HC908-on-Mac-OS-X-SDCC-Eclipse/m-p/204950#M17068</guid>
      <dc:creator>robertrau</dc:creator>
      <dc:date>2011-09-04T00:07:56Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up a Free tool chain for HC908 on Mac OS X: SDCC,Eclipse,make and a Free bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Setting-up-a-Free-tool-chain-for-HC908-on-Mac-OS-X-SDCC-Eclipse/m-p/204951#M17069</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bob,&lt;/P&gt;&lt;P&gt;I just tried sdcc 3.1 with a S08js16.&lt;/P&gt;&lt;P&gt;For the JS16 the compile line should contain -mhc08 --data-loc 0x80 --code-loc 0xC400 --stack-loc 0x027F&lt;/P&gt;&lt;P&gt;interesting enough the stack-loc must be in the compile stage (not the linker as it does nothing there).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For flashing, it is likely you can port usbdm without much effort (based on wxwidgets and libusb which are both available on mac).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Feb 2012 12:21:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Setting-up-a-Free-tool-chain-for-HC908-on-Mac-OS-X-SDCC-Eclipse/m-p/204951#M17069</guid>
      <dc:creator>ggorlik</dc:creator>
      <dc:date>2012-02-13T12:21:08Z</dc:date>
    </item>
  </channel>
</rss>