<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CT_Bias Timing in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CT-Bias-Timing/m-p/204927#M17062</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi all,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Is there any way to adjust the time between the change of state of CT_Bias pin (in MC13213) and the start of transmission/reception?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I´m using Beestack and I´m almost sure that this is impossible to do via software. And I can´t find&amp;nbsp;any register to do that. Anyone knows?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If the time of switching CT_Bias is fixed, I think that there is some time to warmup and some time to warmdown (after transmission), am I right? Anyone knows exactly the time of it? I need that to overcome possible&amp;nbsp;timing issues with an external PA/LNA. Thank you all!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;DedsBee&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Nov 2008 23:42:09 GMT</pubDate>
    <dc:creator>DedsBee</dc:creator>
    <dc:date>2008-11-24T23:42:09Z</dc:date>
    <item>
      <title>CT_Bias Timing</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CT-Bias-Timing/m-p/204927#M17062</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi all,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Is there any way to adjust the time between the change of state of CT_Bias pin (in MC13213) and the start of transmission/reception?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I´m using Beestack and I´m almost sure that this is impossible to do via software. And I can´t find&amp;nbsp;any register to do that. Anyone knows?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If the time of switching CT_Bias is fixed, I think that there is some time to warmup and some time to warmdown (after transmission), am I right? Anyone knows exactly the time of it? I need that to overcome possible&amp;nbsp;timing issues with an external PA/LNA. Thank you all!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;DedsBee&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Nov 2008 23:42:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/CT-Bias-Timing/m-p/204927#M17062</guid>
      <dc:creator>DedsBee</dc:creator>
      <dc:date>2008-11-24T23:42:09Z</dc:date>
    </item>
    <item>
      <title>Re: CT_Bias Timing</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CT-Bias-Timing/m-p/204928#M17063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;I do not know of a way to change the timing of CT_BIAS.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;gt; I think that there is some time to warmup and some time to warmdown (after transmission), am I right?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I measured some of this for CT_BIAS&amp;nbsp;here:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;A href="http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;message.id=12549#M12549" target="_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&amp;amp;message.id=12549#M12549&lt;/A&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;That seemed to confirm what was in MC13202RM.pdf in section 3.10.3.1.3:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;B&gt;&lt;FONT face="Arial"&gt;&lt;B&gt;&lt;FONT face="Arial"&gt;&lt;B&gt;&lt;FONT color="#000000" face="Arial"&gt;&lt;/FONT&gt;&lt;/B&gt;&lt;/FONT&gt;&lt;/B&gt;&lt;/FONT&gt;&lt;/B&gt;&lt;P align="left"&gt;&lt;B&gt;&lt;FONT face="Arial"&gt;&lt;FONT face="Arial"&gt;&lt;FONT color="#000000" face="Arial"&gt;3.10.3.1.3 Modem TX Timing profile&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/B&gt;&lt;/P&gt;&lt;P align="left"&gt;&lt;B&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;The transmit or TX timing profile is more predictable than the RX profile. Figure 3-10 shows the timing&lt;/FONT&gt; &lt;FONT face="Times New Roman"&gt;profile for a TX operation. There is the usual initial 144 μs warm-up period from idle current to full TX&lt;/FONT&gt; &lt;FONT face="Times New Roman"&gt;current (typically 30 mA) followed by the TX operation (TX is covered in detail in&lt;/FONT&gt; &lt;FONT face="Times New Roman"&gt;Section 6.3, “Active&lt;/FONT&gt; &lt;FONT face="Times New Roman"&gt;Modes”&lt;/FONT&gt;&lt;FONT face="Times New Roman"&gt;). The TX time is not a set figure but it is predictable.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/B&gt;&lt;/P&gt;&lt;P align="left"&gt;&lt;B&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;The raw transmission rate of the IEEE 802.15.4 2.4 GHz physical layer is 62.5 ksymbols/s or 250 kb/s.&lt;/FONT&gt; &lt;FONT face="Times New Roman"&gt;This means the TX time for 2 symbols or 1 byte of data is 32 μs. An IEEE 802.15.4 2.4 compliant packet&lt;/FONT&gt; &lt;FONT face="Times New Roman"&gt;has 4 bytes of preamble, 1 byte of SFD, 1 byte of FLI, 2 bytes of FCS plus the payload data (125 bytes&lt;/FONT&gt; &lt;FONT face="Times New Roman"&gt;maximum). As a result the, the overhead of a frame is 8 bytes or 8 x 32 = 256 μs, and the maximum payload&lt;/FONT&gt; &lt;FONT face="Times New Roman"&gt;TX time is 125 x 32 = 4000 μs. The TX time for a packet then is:&lt;/FONT&gt;&lt;/FONT&gt;&lt;/B&gt;&lt;/P&gt;&lt;P align="left"&gt;&lt;B&gt;&lt;FONT color="#000000" face="Times New Roman"&gt;Total TX time (μs) = 256 + (payload bytes x 32)&lt;/FONT&gt;&lt;/B&gt;&lt;/P&gt;&lt;P align="left"&gt;&lt;B&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;The TX operation will end after the FCS bytes are sent. The return to Idle has a “warm down” period of&lt;/FONT&gt; &lt;FONT face="Times New Roman"&gt;10 μs to allow the RF transmitter to taper off in a manner to avoid RF “splatter”.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/B&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Nov 2008 07:21:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/CT-Bias-Timing/m-p/204928#M17063</guid>
      <dc:creator>RichTestardi</dc:creator>
      <dc:date>2008-11-25T07:21:44Z</dc:date>
    </item>
    <item>
      <title>Re: CT_Bias Timing</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/CT-Bias-Timing/m-p/204929#M17064</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Thank you Rich! That´s exactly what I need. 144 us warm-up period is good enough for me to enable the external PA.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks again!&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;DedsBee&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Nov 2008 08:40:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/CT-Bias-Timing/m-p/204929#M17064</guid>
      <dc:creator>DedsBee</dc:creator>
      <dc:date>2008-11-25T08:40:25Z</dc:date>
    </item>
  </channel>
</rss>