<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ZigBee 13213 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-13213/m-p/204890#M17057</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You don't mention what software stack you are using... Simple MAC, 802.15.4MAC, or ZigBee BeeStack.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If you are using ZigBee BeeStack use this:&lt;/DIV&gt;&lt;DIV&gt;void Asp_PortReq(uint8_t portWrite, uint8_t *portValue);&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If not, you need to write the values directly to the ABEL registers 0x3F.&amp;nbsp; See MC1321xRM (reference manual).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;NOTE: Don't foget to set the DDR (Data Direction Register) before hand (during initialization).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;If you are using ZigBee BeeStack use this:&lt;/DIV&gt;&lt;DIV&gt;void&amp;nbsp;&amp;nbsp;&amp;nbsp; Asp_DdrReq(uint8_t directionMask);&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If not, you need to write the values directly to the ABEL registers 0x0B.&amp;nbsp; See MC1321xRM (reference manual).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;WARNING:&amp;nbsp; Messing with the radio's GPIO can cause big problems if you are not careful to avoid the I/O used to interface to the main processor.&amp;nbsp; See MC1321xRM (reference manual).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;- Ware&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Mar 2008 20:20:01 GMT</pubDate>
    <dc:creator>Ware</dc:creator>
    <dc:date>2008-03-25T20:20:01Z</dc:date>
    <item>
      <title>ZigBee 13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-13213/m-p/204889#M17056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN style=": ; font-size: 4; font-family: Arial;"&gt;Hey,&lt;BR /&gt;&lt;BR /&gt;I need help. I need to activate the GPIO pin on the SRB and control using the NRB. I have no idea how to do this &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif"&gt;&lt;IMG alt=":smileysad:" class="emoticon emoticon-smileysad" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif" title="Smiley Sad" /&gt;&lt;/A&gt;&amp;nbsp; can anyone help me?&lt;BR /&gt;&lt;/SPAN&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Mar 2008 09:17:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-13213/m-p/204889#M17056</guid>
      <dc:creator>zulfahmiamran</dc:creator>
      <dc:date>2008-03-21T09:17:21Z</dc:date>
    </item>
    <item>
      <title>Re: ZigBee 13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-13213/m-p/204890#M17057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;You don't mention what software stack you are using... Simple MAC, 802.15.4MAC, or ZigBee BeeStack.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If you are using ZigBee BeeStack use this:&lt;/DIV&gt;&lt;DIV&gt;void Asp_PortReq(uint8_t portWrite, uint8_t *portValue);&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If not, you need to write the values directly to the ABEL registers 0x3F.&amp;nbsp; See MC1321xRM (reference manual).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;NOTE: Don't foget to set the DDR (Data Direction Register) before hand (during initialization).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;If you are using ZigBee BeeStack use this:&lt;/DIV&gt;&lt;DIV&gt;void&amp;nbsp;&amp;nbsp;&amp;nbsp; Asp_DdrReq(uint8_t directionMask);&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If not, you need to write the values directly to the ABEL registers 0x0B.&amp;nbsp; See MC1321xRM (reference manual).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;WARNING:&amp;nbsp; Messing with the radio's GPIO can cause big problems if you are not careful to avoid the I/O used to interface to the main processor.&amp;nbsp; See MC1321xRM (reference manual).&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;- Ware&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Mar 2008 20:20:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-13213/m-p/204890#M17057</guid>
      <dc:creator>Ware</dc:creator>
      <dc:date>2008-03-25T20:20:01Z</dc:date>
    </item>
    <item>
      <title>Re: ZigBee 13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-13213/m-p/204891#M17058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hey,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks for the reply. I'm using the Freescale Beekit. For the solution, i am trying to control the GPIO port to be HIGH (1) or LOW (0) such that this could be connected to my hardware.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I&amp;nbsp;am using the 1321XNSK with one NCB board and 2 SRB board. How can I control this? i've tried looking ath eht MC1321XSRB header file but i dont understand the the pin.. ie MC13192_RESET which has been redefine from PTDD_PTDD3. I do not find this pin anywhere on my data sheet.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Please Help..&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;using Codewarrior IDE version 5.9.0&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Apr 2008 13:20:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-13213/m-p/204891#M17058</guid>
      <dc:creator>zulfahmiamran</dc:creator>
      <dc:date>2008-04-01T13:20:01Z</dc:date>
    </item>
    <item>
      <title>Re: ZigBee 13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-13213/m-p/204892#M17059</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The code below is not tested... but something like this should work:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV class="msg_source_code"&gt;&lt;DIV class="text_smallest"&gt;Code:&lt;/DIV&gt;&lt;PRE&gt;#include "AppAspINTERFACE.h"// inside of init routineAsp_DdrReq(0x08);   // make GPIO4 an output// to write logic HIGHpVal = 0x08;  // logic HIGH on GPIO4Asp_PortReq(TRUE, &amp;amp;pVal);  // write pVal to GPIO// to write logic LOWpVal = 0;  // logic LOW on GPIO4Asp_PortReq(TRUE, &amp;amp;pVal);  // write pVal to GPIO&lt;/PRE&gt;&lt;/DIV&gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Apr 2008 00:14:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ZigBee-13213/m-p/204892#M17059</guid>
      <dc:creator>Ware</dc:creator>
      <dc:date>2008-04-04T00:14:12Z</dc:date>
    </item>
  </channel>
</rss>