<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 9S08JM Pullup with External TPMCLK in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08JM-Pullup-with-External-TPMCLK/m-p/204750#M17040</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;I am using the IRQ/TPMCLK pin for an external clock input to TPM2 (TPM2SC = 0x18). It appears this combination disables the internal pullup but I cannot find confirmation in the documentation. I have tried setting IRQSC_IRQPE=1 but it has no effect.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I can add an external pullup (this is a prototype) but I'd like to be sure I'm not missing something. Can anyone confirm this behavior or suggest how to enable the internal pullup with this configuration? Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Dave&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;P.S.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The external clock source comes though a blocking diode. That's why I need the pullup.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Mar 2008 00:24:54 GMT</pubDate>
    <dc:creator>dp</dc:creator>
    <dc:date>2008-03-21T00:24:54Z</dc:date>
    <item>
      <title>9S08JM Pullup with External TPMCLK</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08JM-Pullup-with-External-TPMCLK/m-p/204750#M17040</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;I am using the IRQ/TPMCLK pin for an external clock input to TPM2 (TPM2SC = 0x18). It appears this combination disables the internal pullup but I cannot find confirmation in the documentation. I have tried setting IRQSC_IRQPE=1 but it has no effect.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I can add an external pullup (this is a prototype) but I'd like to be sure I'm not missing something. Can anyone confirm this behavior or suggest how to enable the internal pullup with this configuration? Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Dave&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;P.S.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The external clock source comes though a blocking diode. That's why I need the pullup.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Mar 2008 00:24:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08JM-Pullup-with-External-TPMCLK/m-p/204750#M17040</guid>
      <dc:creator>dp</dc:creator>
      <dc:date>2008-03-21T00:24:54Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08JM Pullup with External TPMCLK</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08JM-Pullup-with-External-TPMCLK/m-p/204751#M17041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi dp,&lt;BR /&gt;&lt;BR /&gt;I believe that the pulling device is only available when the IRQ function is active (IRQSC:IRQPE=1). There is no other way to enable pulling devices when this pin is operating as TPMCLK input (as it is not mapped to any&amp;nbsp; PTxPE bit).&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Mar 2008 05:29:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08JM-Pullup-with-External-TPMCLK/m-p/204751#M17041</guid>
      <dc:creator>fabio</dc:creator>
      <dc:date>2008-03-21T05:29:01Z</dc:date>
    </item>
    <item>
      <title>Re: 9S08JM Pullup with External TPMCLK</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08JM-Pullup-with-External-TPMCLK/m-p/204752#M17042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The spec says:&lt;BR /&gt;"The IRQ pin, when enabled, defaults to use an internal pull device (IRQPDD = 0), the device is a pullup&lt;BR /&gt;or pull-down depending on the polarity chosen"&lt;BR /&gt;&lt;BR /&gt;So if it &lt;I&gt;disabled&lt;/I&gt;, then the pull up is &lt;I&gt;not&lt;/I&gt; connected.&lt;BR /&gt;&lt;BR /&gt;Also note that this in not a pin that is shared with a GPIO, pins that are shared with a GPIO usually can use the pull up/pull downs. If you look at the block diagram, you will see signals coming in thru a port. Generally these signal are buffer by the port. This is not one of these signals.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Mar 2008 06:31:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08JM-Pullup-with-External-TPMCLK/m-p/204752#M17042</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-03-21T06:31:57Z</dc:date>
    </item>
  </channel>
</rss>