<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Which Bootloader in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-Bootloader/m-p/204622#M17019</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I conviently failed to mention I am using an MC9S08JM60.&amp;nbsp; Sorry about that.&amp;nbsp; Working with the demoJM board at the moment.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Jun 2010 02:27:45 GMT</pubDate>
    <dc:creator>Yoheeb</dc:creator>
    <dc:date>2010-06-02T02:27:45Z</dc:date>
    <item>
      <title>Which Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-Bootloader/m-p/204621#M17018</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have managed to wedge my app inside the CMX gernic hid demo application.&amp;nbsp; WHile not the cleanest way to go, it was quick and dirty for what I needed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My question now is, which bootloader do I wedge into it?&amp;nbsp; I have seen posts for both the AN3561 and the AN 2295.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, I am putting this in place backwards, since it would of been easier to create a project from scratch using either one as a template, so would either of these be easier to jam in?&amp;nbsp; or am I even asking the right question here?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I do need to program over USB, the host system is controlled, so we can make sure all appropriate drivers will be in place, it need not be a CDC-HID, it can be anything.&amp;nbsp; Also, invoking the bootloader by jumpering an input is fine, it isn't required to be invoked remotely, although I wouldn't discard that option if it were there.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yoheeb&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jun 2010 02:24:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-Bootloader/m-p/204621#M17018</guid>
      <dc:creator>Yoheeb</dc:creator>
      <dc:date>2010-06-02T02:24:20Z</dc:date>
    </item>
    <item>
      <title>Re: Which Bootloader</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-Bootloader/m-p/204622#M17019</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I conviently failed to mention I am using an MC9S08JM60.&amp;nbsp; Sorry about that.&amp;nbsp; Working with the demoJM board at the moment.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jun 2010 02:27:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Which-Bootloader/m-p/204622#M17019</guid>
      <dc:creator>Yoheeb</dc:creator>
      <dc:date>2010-06-02T02:27:45Z</dc:date>
    </item>
  </channel>
</rss>