<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: S08DZ32 MSCAN not Syncing</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08DZ32-MSCAN-not-Syncing/m-p/203776#M16900</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i think you should check the configuration of the hardware.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if you are using the high-speed CAN, both H and L should be at 2.5V in idle. you could use pull-up and pull-down to realize it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Jun 2010 11:06:37 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2010-06-04T11:06:37Z</dc:date>
    <item>
      <title>S08DZ32 MSCAN not Syncing</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08DZ32-MSCAN-not-Syncing/m-p/203775#M16899</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I run the same small test code for MSCAN on the S08DZ60 Demo Board&amp;nbsp;as on my target board running a S08DZ32. On the demo board I get the sync bit, but on my target I do not. I am using&amp;nbsp;the TI ISO1050 Isolated CAN Transceiver on my target. The RXCAN and TXCAN MPU pins are at logic high while CAN Bus is not connected. (5 VDC)&amp;nbsp;I am stuck for an answer on why the MSCAN is not syncing. BTW, MSCAN initialization is working fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;TIA,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 May 2010 04:58:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08DZ32-MSCAN-not-Syncing/m-p/203775#M16899</guid>
      <dc:creator>datamstr</dc:creator>
      <dc:date>2010-05-29T04:58:37Z</dc:date>
    </item>
    <item>
      <title>Re: S08DZ32 MSCAN not Syncing</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08DZ32-MSCAN-not-Syncing/m-p/203776#M16900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i think you should check the configuration of the hardware.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if you are using the high-speed CAN, both H and L should be at 2.5V in idle. you could use pull-up and pull-down to realize it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jun 2010 11:06:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08DZ32-MSCAN-not-Syncing/m-p/203776#M16900</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2010-06-04T11:06:37Z</dc:date>
    </item>
    <item>
      <title>Re: S08DZ32 MSCAN not Syncing</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08DZ32-MSCAN-not-Syncing/m-p/203777#M16901</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry, i mistake the pin of MCU for CAN interface&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jun 2010 11:08:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08DZ32-MSCAN-not-Syncing/m-p/203777#M16901</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2010-06-04T11:08:36Z</dc:date>
    </item>
  </channel>
</rss>