<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックJaMini USB Microcontroller Module (40 pin DIP package with MC9S08JM60)</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JaMini-USB-Microcontroller-Module-40-pin-DIP-package-with/m-p/202771#M16711</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just wanted to let everyone know that we have launched a new module based around the Freescale JM microcontroller family. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please visit us at &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.protoease.com" rel="nofollow" target="_blank"&gt;http://www.protoease.com&lt;/A&gt; for details.&amp;nbsp; On the blog link, you can find the full schematic of the module's internals.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A quick summary of features:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Uses the Freescale MC9S08JM60 microcontroller with 60 KB Flash and 4 KB RAM&lt;/LI&gt;&lt;LI&gt;Size of a 40-pin DIP IC, uses standard 0.1" C-C pin headers (or you can direct wire to it)&lt;/LI&gt;&lt;LI&gt;Includes Mini-USB connection - create a USB device with the module or use it to load code without a debugger!&lt;/LI&gt;&lt;LI&gt;Includes LDO voltage regulator supporting up to 16V input.&amp;nbsp; Output (up to 1 A) can be used to power user's circuit.&lt;/LI&gt;&lt;LI&gt;Includes crystal and all other support components for the microcontroller&lt;/LI&gt;&lt;LI&gt;Breaks out all I/O to the pin headers (with exception of a few I/O lines).&lt;/LI&gt;&lt;LI&gt;Includes two pushbuttons: Reset and BOOT/User.&amp;nbsp; The BOOT button can be used to enter Bootloader mode, whereby code can be flashed to the micro over the USB connection.&lt;/LI&gt;&lt;LI&gt;BDM connection is included but not populated&lt;/LI&gt;&lt;/UL&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hopefully this will help someone prototype their idea easier and faster. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Aaron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Sep 2012 14:35:08 GMT</pubDate>
    <dc:creator>protoease</dc:creator>
    <dc:date>2012-09-27T14:35:08Z</dc:date>
    <item>
      <title>JaMini USB Microcontroller Module (40 pin DIP package with MC9S08JM60)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/JaMini-USB-Microcontroller-Module-40-pin-DIP-package-with/m-p/202771#M16711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just wanted to let everyone know that we have launched a new module based around the Freescale JM microcontroller family. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please visit us at &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.protoease.com" rel="nofollow" target="_blank"&gt;http://www.protoease.com&lt;/A&gt; for details.&amp;nbsp; On the blog link, you can find the full schematic of the module's internals.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A quick summary of features:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Uses the Freescale MC9S08JM60 microcontroller with 60 KB Flash and 4 KB RAM&lt;/LI&gt;&lt;LI&gt;Size of a 40-pin DIP IC, uses standard 0.1" C-C pin headers (or you can direct wire to it)&lt;/LI&gt;&lt;LI&gt;Includes Mini-USB connection - create a USB device with the module or use it to load code without a debugger!&lt;/LI&gt;&lt;LI&gt;Includes LDO voltage regulator supporting up to 16V input.&amp;nbsp; Output (up to 1 A) can be used to power user's circuit.&lt;/LI&gt;&lt;LI&gt;Includes crystal and all other support components for the microcontroller&lt;/LI&gt;&lt;LI&gt;Breaks out all I/O to the pin headers (with exception of a few I/O lines).&lt;/LI&gt;&lt;LI&gt;Includes two pushbuttons: Reset and BOOT/User.&amp;nbsp; The BOOT button can be used to enter Bootloader mode, whereby code can be flashed to the micro over the USB connection.&lt;/LI&gt;&lt;LI&gt;BDM connection is included but not populated&lt;/LI&gt;&lt;/UL&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hopefully this will help someone prototype their idea easier and faster. &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Aaron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Sep 2012 14:35:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/JaMini-USB-Microcontroller-Module-40-pin-DIP-package-with/m-p/202771#M16711</guid>
      <dc:creator>protoease</dc:creator>
      <dc:date>2012-09-27T14:35:08Z</dc:date>
    </item>
  </channel>
</rss>