<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: HCS08QG8 UART: mix C and Assembly in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08QG8-UART-mix-C-and-Assembly/m-p/202757#M16708</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are a few reasons why your code will not compile without error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Firstly, I assume that you have already defined ACK and T100MS as numeric macros?&amp;nbsp; How have you defined the macro ILOP, since this is one of the problem areas?&amp;nbsp; I also notice that you have&amp;nbsp;used ILOP as a label name, as well as a macro name.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You are assuming that the macro SCIS1_RDRF represents a bit number.&amp;nbsp; In fact, the macro identifies a component of a bit field, and is normally used in the context of ... if (SCIS1_RDRF)&amp;nbsp; {&amp;nbsp;&amp;nbsp; }&amp;nbsp;&amp;nbsp; You will presumably need to define your own macro to represent the bit number for the&amp;nbsp;RDRF bit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When a C function is called via inline assembly, the empty parameter braces should not be included.&amp;nbsp; Additionally, you should call&amp;nbsp;using JSR, rather than BSR, because you do not know the precise location of the C function code.&amp;nbsp; If the C function requires any parameters, or returns a value, the assembly code would need to take into account the C calling convention for the MCU type.&amp;nbsp; If this is the case, it is sometimes less error prone to make use of global variables for the passing of values.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I assume that your inline code forms part of a separate function?&amp;nbsp; It must not be placed directly within main() because of the presence of the RTS instruction (and main() must never exit).&amp;nbsp; Actually, the final RTS is not required because the compiler will automatically provide the RTS when it exits the function.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Finally, I would tend to convert all binary numbers to hexadecimal format as it is possible that some compilers will not recognise the binary format.&amp;nbsp; It is my understanding that ANSI C does not include&amp;nbsp;binary numbers - maybe others can clarify this aspect.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 May 2011 14:52:25 GMT</pubDate>
    <dc:creator>bigmac</dc:creator>
    <dc:date>2011-05-03T14:52:25Z</dc:date>
    <item>
      <title>HCS08QG8 UART: mix C and Assembly</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08QG8-UART-mix-C-and-Assembly/m-p/202756#M16707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am adding a serial feature to a previous written C codes.&amp;nbsp; The serial code is in assembly that i obtained from (AN2295SW). I understand that assembly codes in C file don't behave the same as "standard" assembly file. Could anyone give me some suggestions on what i need to modify to get this piece of code up and running. Another question is can i branch to a "regular" C function within the asm brackets ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am currently using CodeWarrior MCU 6.3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;asm&amp;nbsp;&amp;nbsp; {&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MOV&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0b00001100,SCIC2;&amp;nbsp;&amp;nbsp; // transmit &amp;amp; receive enable&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CLR&amp;nbsp;&amp;nbsp; SCIBDH;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MOV&amp;nbsp;&amp;nbsp; #26, SCIBDL;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //BUS (8.0M)/(16 *26) = 19200Bd&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CLR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SCIC3;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // clear SCIC3&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LDA&amp;nbsp;&amp;nbsp; SCIS1;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Load Accumulator A with SCIS1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MOV&amp;nbsp;&amp;nbsp; #ACK, SCID;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Move from SCID to ACK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LDX&amp;nbsp;&amp;nbsp; #T100MS;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Load Accumulator X with 100ms&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; L2:&amp;nbsp;&amp;nbsp; CLRA;&amp;nbsp;&amp;nbsp;&amp;nbsp; L1:&amp;nbsp;&amp;nbsp; BRSET&amp;nbsp;&amp;nbsp; SCIS1_RDRF,SCIS1,CAUGHT; //Branch to "CAUGHT" if SCIIS1_RDRF is&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DBNZA&amp;nbsp;&amp;nbsp; L1; //Decrement A and Branch to "L1" if not Zero&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DBNZX&amp;nbsp;&amp;nbsp; L2; //Decrement X and Branch to "L2" if not Zero&amp;nbsp;&amp;nbsp;&amp;nbsp; ILOP:&amp;nbsp;&amp;nbsp;&amp;nbsp; //&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; timeout&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ILOP;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //generate RESET by doing illegal operation&amp;nbsp;&amp;nbsp;&amp;nbsp; CAUGHT:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // CAUGHT IN SELF-PROGRAMMING?&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BSR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; READ1;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Branch to "READ"&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CBEQA&amp;nbsp;&amp;nbsp; #ACK, SUCC;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Got ACK! or&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ILOP;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //generate RESET by doing illegal operation&amp;nbsp;&amp;nbsp;&amp;nbsp; SUCC:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LDA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #ACK;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BSR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Serial();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //functions that handles serial commands&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; READ1:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BRCLR&amp;nbsp;&amp;nbsp; SCIS1_RDRF,SCIS1,READ1;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LDA&amp;nbsp;&amp;nbsp; SCID;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RTS;&amp;nbsp; }&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;I get the following error messages after each compiling the codes&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18113: Bitno expected&lt;BR /&gt;main.c line 1117&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18101: Object is not a field&lt;BR /&gt;main.c line 1117&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18110: Comma expected&lt;BR /&gt;main.c line 1117&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18123: end of line expected&lt;BR /&gt;main.c line 1117&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18125: Invalid opcode or ':' expected&lt;BR /&gt;main.c line 1122&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18125: Invalid opcode or ':' expected&lt;BR /&gt;main.c line 1126&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18123: end of line expected&lt;BR /&gt;main.c line 1129&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18101: Object is not a field&lt;BR /&gt;main.c line 1134&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18113: Bitno expected&lt;BR /&gt;main.c line 1134&amp;nbsp; &amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18110: Comma expected&lt;BR /&gt;main.c line 1134&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18110: Comma expected&lt;BR /&gt;main.c line 1134&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18103: Factor expected&lt;BR /&gt;main.c line 1134&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18123: end of line expected&lt;BR /&gt;main.c line 1134&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18101: Object is not a field&lt;BR /&gt;main.c line 1135&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18123: end of line expected&lt;BR /&gt;main.c line 1135&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18000: Label not set&lt;BR /&gt;main.c line 1134&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : C18000: Label not set&lt;BR /&gt;main.c line 1117&amp;nbsp;&amp;nbsp;&lt;BR /&gt;Error&amp;nbsp;&amp;nbsp; : Compile failed&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 May 2011 05:05:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08QG8-UART-mix-C-and-Assembly/m-p/202756#M16707</guid>
      <dc:creator>Designer11</dc:creator>
      <dc:date>2011-05-03T05:05:35Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08QG8 UART: mix C and Assembly</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08QG8-UART-mix-C-and-Assembly/m-p/202757#M16708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are a few reasons why your code will not compile without error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Firstly, I assume that you have already defined ACK and T100MS as numeric macros?&amp;nbsp; How have you defined the macro ILOP, since this is one of the problem areas?&amp;nbsp; I also notice that you have&amp;nbsp;used ILOP as a label name, as well as a macro name.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You are assuming that the macro SCIS1_RDRF represents a bit number.&amp;nbsp; In fact, the macro identifies a component of a bit field, and is normally used in the context of ... if (SCIS1_RDRF)&amp;nbsp; {&amp;nbsp;&amp;nbsp; }&amp;nbsp;&amp;nbsp; You will presumably need to define your own macro to represent the bit number for the&amp;nbsp;RDRF bit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When a C function is called via inline assembly, the empty parameter braces should not be included.&amp;nbsp; Additionally, you should call&amp;nbsp;using JSR, rather than BSR, because you do not know the precise location of the C function code.&amp;nbsp; If the C function requires any parameters, or returns a value, the assembly code would need to take into account the C calling convention for the MCU type.&amp;nbsp; If this is the case, it is sometimes less error prone to make use of global variables for the passing of values.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I assume that your inline code forms part of a separate function?&amp;nbsp; It must not be placed directly within main() because of the presence of the RTS instruction (and main() must never exit).&amp;nbsp; Actually, the final RTS is not required because the compiler will automatically provide the RTS when it exits the function.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Finally, I would tend to convert all binary numbers to hexadecimal format as it is possible that some compilers will not recognise the binary format.&amp;nbsp; It is my understanding that ANSI C does not include&amp;nbsp;binary numbers - maybe others can clarify this aspect.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mac&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 May 2011 14:52:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08QG8-UART-mix-C-and-Assembly/m-p/202757#M16708</guid>
      <dc:creator>bigmac</dc:creator>
      <dc:date>2011-05-03T14:52:25Z</dc:date>
    </item>
  </channel>
</rss>