<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックAN2295 - Store a few byte in protected memory ( Serial Number)</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-Store-a-few-byte-in-protected-memory-Serial-Number/m-p/202317#M16617</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the serial bootloader to flash my app to a MC9S08AW32&amp;nbsp;. Works like perfect.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, now I have the request to store a serial number in protected memory - just 2 or 4 bytes would be plenty.&lt;/P&gt;&lt;P&gt;My understanding is that the bootloader sets the flash protectioin flags to protect itself - So I would need to "issue" and flash the serial number when the bootloader itself is initially flashed, correct ?&lt;/P&gt;&lt;P&gt;Which in turn would require to modify the bootloader code and memory layout ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are my thoughts remotely correct? Any hints are highly appreciated&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;( Coming from the win32 world ... dealing with bits and bytes is not that esy for me &lt;SPAN aria-label="Happy" class="emoticon_happy emoticon-inline" style="height:16px;width:16px;"&gt;&lt;/SPAN&gt; )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Oskar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 30 Apr 2011 02:51:11 GMT</pubDate>
    <dc:creator>oskaratk</dc:creator>
    <dc:date>2011-04-30T02:51:11Z</dc:date>
    <item>
      <title>AN2295 - Store a few byte in protected memory ( Serial Number)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-Store-a-few-byte-in-protected-memory-Serial-Number/m-p/202317#M16617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the serial bootloader to flash my app to a MC9S08AW32&amp;nbsp;. Works like perfect.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, now I have the request to store a serial number in protected memory - just 2 or 4 bytes would be plenty.&lt;/P&gt;&lt;P&gt;My understanding is that the bootloader sets the flash protectioin flags to protect itself - So I would need to "issue" and flash the serial number when the bootloader itself is initially flashed, correct ?&lt;/P&gt;&lt;P&gt;Which in turn would require to modify the bootloader code and memory layout ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are my thoughts remotely correct? Any hints are highly appreciated&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;( Coming from the win32 world ... dealing with bits and bytes is not that esy for me &lt;SPAN aria-label="Happy" class="emoticon_happy emoticon-inline" style="height:16px;width:16px;"&gt;&lt;/SPAN&gt; )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Oskar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Apr 2011 02:51:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-Store-a-few-byte-in-protected-memory-Serial-Number/m-p/202317#M16617</guid>
      <dc:creator>oskaratk</dc:creator>
      <dc:date>2011-04-30T02:51:11Z</dc:date>
    </item>
    <item>
      <title>Re: AN2295 - Store a few byte in protected memory ( Serial Number)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-Store-a-few-byte-in-protected-memory-Serial-Number/m-p/202318#M16618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi P&amp;amp;E cyclonepro have program serial number function. for you information.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Apr 2011 21:33:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN2295-Store-a-few-byte-in-protected-memory-Serial-Number/m-p/202318#M16618</guid>
      <dc:creator>Mickey</dc:creator>
      <dc:date>2011-04-30T21:33:41Z</dc:date>
    </item>
  </channel>
</rss>