<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic M9S08JM60 design opinion sought. in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M9S08JM60-design-opinion-sought/m-p/200962#M16451</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have settled on the S08JM60 for a simple design.&amp;nbsp; The device needs to communicate via usb to a host PC.&amp;nbsp; It needs to do gpio, and some A/D.&amp;nbsp; There is not very much trafic back and forth, the speeds of the activities are measured in seconds.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Should I just use this device as a HID, and just use the demo firmware and pc side software as a big starting platform, or should I make this a more "complete" usb device.&amp;nbsp; I might not even have to store anything in flash in terms of data.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Longer term, I'd like to eventually generalize this, add an OS and make it a more robust usb device, but at the moment, just need to hit the ground running.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have never done USB related work, so just looking for a quick "up and running" approach.&amp;nbsp; I need to handle a couple switches, output to some relays, read a couple photo-detects, send info back to pc every few seconds.&amp;nbsp; probably a heartbeat of somekind to the host.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyway, thanks for the thoughts.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 May 2010 01:46:03 GMT</pubDate>
    <dc:creator>Yoheeb</dc:creator>
    <dc:date>2010-05-18T01:46:03Z</dc:date>
    <item>
      <title>M9S08JM60 design opinion sought.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M9S08JM60-design-opinion-sought/m-p/200962#M16451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have settled on the S08JM60 for a simple design.&amp;nbsp; The device needs to communicate via usb to a host PC.&amp;nbsp; It needs to do gpio, and some A/D.&amp;nbsp; There is not very much trafic back and forth, the speeds of the activities are measured in seconds.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Should I just use this device as a HID, and just use the demo firmware and pc side software as a big starting platform, or should I make this a more "complete" usb device.&amp;nbsp; I might not even have to store anything in flash in terms of data.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Longer term, I'd like to eventually generalize this, add an OS and make it a more robust usb device, but at the moment, just need to hit the ground running.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have never done USB related work, so just looking for a quick "up and running" approach.&amp;nbsp; I need to handle a couple switches, output to some relays, read a couple photo-detects, send info back to pc every few seconds.&amp;nbsp; probably a heartbeat of somekind to the host.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyway, thanks for the thoughts.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 May 2010 01:46:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/M9S08JM60-design-opinion-sought/m-p/200962#M16451</guid>
      <dc:creator>Yoheeb</dc:creator>
      <dc:date>2010-05-18T01:46:03Z</dc:date>
    </item>
    <item>
      <title>Re: M9S08JM60 design opinion sought.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/M9S08JM60-design-opinion-sought/m-p/200963#M16452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I went with a HID, in case anyone was following this.&amp;nbsp; For what I need, the speeds and amount of data are trvially small, so this was plenty.&amp;nbsp; I was even able to basically wrap the existing sample code out there to get a functional prototype.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to go back and do some actual code design and clean it all up, but that wasn't the goal for the first few days.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks to all those who have posted code/forum responses, etc. which I used extensively to get the ball rolling.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 May 2010 21:23:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/M9S08JM60-design-opinion-sought/m-p/200963#M16452</guid>
      <dc:creator>Yoheeb</dc:creator>
      <dc:date>2010-05-20T21:23:32Z</dc:date>
    </item>
  </channel>
</rss>