<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SD Card / SPI Assistance Needed in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SD-Card-SPI-Assistance-Needed/m-p/200303#M16350</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm using an&amp;nbsp; HCS08LG32, running at 3.3V to interface with an SD card via SPI.&amp;nbsp; CLK frequency is at 4M, which is divided by 12 for the SPI SD card init sequence.&amp;nbsp; Most of the code is borrowed from that provided with the JM60 USB/SDcard demo.&amp;nbsp; I get thru the init() sequence most (by not all times) and get an error most of the time in writing the SD card.&amp;nbsp; I seem to be able to read the SD "most" of the time.&amp;nbsp; In the rare occasions&amp;nbsp;that a write is successful, I can read back the numbers written.&amp;nbsp; &amp;nbsp;I have the SW code as an attachment here.&lt;/P&gt;&lt;P&gt;Any suggestions welcome.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 15 May 2010 05:13:44 GMT</pubDate>
    <dc:creator>Thunder</dc:creator>
    <dc:date>2010-05-15T05:13:44Z</dc:date>
    <item>
      <title>SD Card / SPI Assistance Needed</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SD-Card-SPI-Assistance-Needed/m-p/200303#M16350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm using an&amp;nbsp; HCS08LG32, running at 3.3V to interface with an SD card via SPI.&amp;nbsp; CLK frequency is at 4M, which is divided by 12 for the SPI SD card init sequence.&amp;nbsp; Most of the code is borrowed from that provided with the JM60 USB/SDcard demo.&amp;nbsp; I get thru the init() sequence most (by not all times) and get an error most of the time in writing the SD card.&amp;nbsp; I seem to be able to read the SD "most" of the time.&amp;nbsp; In the rare occasions&amp;nbsp;that a write is successful, I can read back the numbers written.&amp;nbsp; &amp;nbsp;I have the SW code as an attachment here.&lt;/P&gt;&lt;P&gt;Any suggestions welcome.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 May 2010 05:13:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SD-Card-SPI-Assistance-Needed/m-p/200303#M16350</guid>
      <dc:creator>Thunder</dc:creator>
      <dc:date>2010-05-15T05:13:44Z</dc:date>
    </item>
    <item>
      <title>Re: SD Card / SPI Assistance Needed</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/SD-Card-SPI-Assistance-Needed/m-p/200304#M16351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I finally located my problem, that being a typo in one of the SPI commands (writing SPIS instead of SPID in a line of code).&amp;nbsp; Everything working fine now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 May 2010 04:19:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/SD-Card-SPI-Assistance-Needed/m-p/200304#M16351</guid>
      <dc:creator>Thunder</dc:creator>
      <dc:date>2010-05-19T04:19:10Z</dc:date>
    </item>
  </channel>
</rss>