<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックCannot Measure Target Baudrate When Programming 908QC16 TSSOP</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Cannot-Measure-Target-Baudrate-When-Programming-908QC16-TSSOP/m-p/200148#M16333</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I recently modified a DEMO908QB8 board by removing the resident processor and adding a connector to an adapter board that allows me to program 'QC16'&amp;nbsp;20-pin SOIC and TSSOP devices.&amp;nbsp; The SOIC devices consistently program without any problems.&amp;nbsp; However, with the TSSOP devices, the programmer initially connects and reports that the device responded properly but always stops and reports that it "could not measure target baudrate."&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Both sockets are correctly wired for the different pinouts of each package type and the signals to either device look fine on a scope.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Do the TSSOP devices require a different programming algorithm or is there something in the literature that I have overlooked?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Any additional insight will be greatly appreciated.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 07 Mar 2008 00:47:58 GMT</pubDate>
    <dc:creator>MrWizard</dc:creator>
    <dc:date>2008-03-07T00:47:58Z</dc:date>
    <item>
      <title>Cannot Measure Target Baudrate When Programming 908QC16 TSSOP</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Cannot-Measure-Target-Baudrate-When-Programming-908QC16-TSSOP/m-p/200148#M16333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I recently modified a DEMO908QB8 board by removing the resident processor and adding a connector to an adapter board that allows me to program 'QC16'&amp;nbsp;20-pin SOIC and TSSOP devices.&amp;nbsp; The SOIC devices consistently program without any problems.&amp;nbsp; However, with the TSSOP devices, the programmer initially connects and reports that the device responded properly but always stops and reports that it "could not measure target baudrate."&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Both sockets are correctly wired for the different pinouts of each package type and the signals to either device look fine on a scope.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Do the TSSOP devices require a different programming algorithm or is there something in the literature that I have overlooked?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Any additional insight will be greatly appreciated.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Mar 2008 00:47:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Cannot-Measure-Target-Baudrate-When-Programming-908QC16-TSSOP/m-p/200148#M16333</guid>
      <dc:creator>MrWizard</dc:creator>
      <dc:date>2008-03-07T00:47:58Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot Measure Target Baudrate When Programming 908QC16 TSSOP</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Cannot-Measure-Target-Baudrate-When-Programming-908QC16-TSSOP/m-p/200149#M16334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I can given a solid answer to the question of flash programming - No they are exactly the same.&lt;BR /&gt;If fact the same device in a different package has exactly the same specifications.&lt;BR /&gt;&lt;BR /&gt;From experience in&amp;nbsp; building prototypes, you might consider that the TSSOP is much finer pitch that the SOIC, and a careful inspection may reveal a small solder bridge between pins and or a pin not completely soldered.&lt;BR /&gt;&lt;BR /&gt;Hopefully you have or have access to a microscope, like around 7x. Inspect from the side, as solder bridges can escape detection when viewed only from the top side.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Mar 2008 02:12:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Cannot-Measure-Target-Baudrate-When-Programming-908QC16-TSSOP/m-p/200149#M16334</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-03-07T02:12:25Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot Measure Target Baudrate When Programming 908QC16 TSSOP</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Cannot-Measure-Target-Baudrate-When-Programming-908QC16-TSSOP/m-p/200150#M16335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Jim -&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks for the info - I was pretty sure that all family members&amp;nbsp;are created equal, but ever hopeful that the problem was not on my end.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The solder joints to the prototype adapter boards look good - the problem may be related to ESD or power supply problems.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Mar 2008 08:20:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Cannot-Measure-Target-Baudrate-When-Programming-908QC16-TSSOP/m-p/200150#M16335</guid>
      <dc:creator>MrWizard</dc:creator>
      <dc:date>2008-03-07T08:20:11Z</dc:date>
    </item>
  </channel>
</rss>