<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックProgramming MC68HC908QY4A</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-MC68HC908QY4A/m-p/199861#M16300</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Is it possible to loas s-record into flash of the QY4A without using usb-Mon-08 from P&amp;amp;E or cyclone pro.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to use monitor mode entry ckt available in datasheet to program the flash of controller.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The security feature is very confusing in it.It says that to load data into flash the security bits has to be entered into flash&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;locations FFF6-FFFD,but these locations are ISR vector addresses.Please some could clarify on these things.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 May 2010 23:27:47 GMT</pubDate>
    <dc:creator>madhub</dc:creator>
    <dc:date>2010-05-12T23:27:47Z</dc:date>
    <item>
      <title>Programming MC68HC908QY4A</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-MC68HC908QY4A/m-p/199861#M16300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Is it possible to loas s-record into flash of the QY4A without using usb-Mon-08 from P&amp;amp;E or cyclone pro.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible to use monitor mode entry ckt available in datasheet to program the flash of controller.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The security feature is very confusing in it.It says that to load data into flash the security bits has to be entered into flash&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;locations FFF6-FFFD,but these locations are ISR vector addresses.Please some could clarify on these things.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 May 2010 23:27:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-MC68HC908QY4A/m-p/199861#M16300</guid>
      <dc:creator>madhub</dc:creator>
      <dc:date>2010-05-12T23:27:47Z</dc:date>
    </item>
    <item>
      <title>Re: Programming MC68HC908QY4A</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-MC68HC908QY4A/m-p/199862#M16301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello and welcome to the fora madhub.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes this is possible.&lt;/P&gt;&lt;P&gt;To get past security you must send the same value as is programmed into these vector locations at the appropriate time.&lt;/P&gt;&lt;P&gt;You can get a free programme to do this from &lt;A href="http://www.pemicro.com/support/download_processor.cfm" rel="nofollow" target="_self"&gt;here&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 May 2010 04:57:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-MC68HC908QY4A/m-p/199862#M16301</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2010-05-13T04:57:04Z</dc:date>
    </item>
  </channel>
</rss>