<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックADC sampling freq. on MC13213</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ADC-sampling-freq-on-MC13213/m-p/199564#M16249</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am trying to figure out the way to set the ADC conversion clock frequency. I have a requirement to sample the analog input at 32KHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Setup&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Using Freescale SRB that is connected to the PC over USB (no wireless connectivity)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. The code is built over SMAC code generated by BeeKit&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3. Setup wherein 1KHz signal is given as input to the ADC(10bits) of MC13213.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4. Buffer this signal and then transmit it over USB to get the data on the machine. (the buffer size is 1200bytes)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;5. ATD1C=0xC1 (ATD control register with Prescaler rate set to 1)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can someone let me know what is the way to set the desired ADC conversion clock frequency? I could not understand the contents of the Table 20.4 of the “MC1321x RM” that refer to the calculations of these frequencies&lt;/SPAN&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Nov 2008 13:59:59 GMT</pubDate>
    <dc:creator>saurabh</dc:creator>
    <dc:date>2008-11-05T13:59:59Z</dc:date>
    <item>
      <title>ADC sampling freq. on MC13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ADC-sampling-freq-on-MC13213/m-p/199564#M16249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am trying to figure out the way to set the ADC conversion clock frequency. I have a requirement to sample the analog input at 32KHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Setup&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Using Freescale SRB that is connected to the PC over USB (no wireless connectivity)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. The code is built over SMAC code generated by BeeKit&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3. Setup wherein 1KHz signal is given as input to the ADC(10bits) of MC13213.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4. Buffer this signal and then transmit it over USB to get the data on the machine. (the buffer size is 1200bytes)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;5. ATD1C=0xC1 (ATD control register with Prescaler rate set to 1)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can someone let me know what is the way to set the desired ADC conversion clock frequency? I could not understand the contents of the Table 20.4 of the “MC1321x RM” that refer to the calculations of these frequencies&lt;/SPAN&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Nov 2008 13:59:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ADC-sampling-freq-on-MC13213/m-p/199564#M16249</guid>
      <dc:creator>saurabh</dc:creator>
      <dc:date>2008-11-05T13:59:59Z</dc:date>
    </item>
    <item>
      <title>Re: ADC sampling freq. on MC13213</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ADC-sampling-freq-on-MC13213/m-p/199565#M16250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;i am also facing the problem for now a month and no one has given a satisfactory answer&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Mar 2010 16:45:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ADC-sampling-freq-on-MC13213/m-p/199565#M16250</guid>
      <dc:creator>Wahab</dc:creator>
      <dc:date>2010-03-17T16:45:37Z</dc:date>
    </item>
  </channel>
</rss>